StripLayoutBuilderToStationType Enumeration

NXOpen.Tooling.StripLayoutBuilder.ToStationType is an alias for NXOpen.Tooling.StripLayoutBuilderToStationType

class NXOpen.Tooling.StripLayoutBuilderToStationType

Bases: object

Specifies the option of To Station for layout

Enum Members

Enum Member Enum Member Description
One
the end layout station is 1
Two
the end layout station is 2
Three
the end layout station is 3
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.