SpreadsheetDataParameter Class

class NXOpen.Tooling.SpreadsheetDataParameter

Bases: NXOpen.TransientObject

Represents parameter in the spreadsheet.

New in version NX8.0.0.

Properties

Property Description
DescriptiveName Returns or sets the descriptive name of the parameter
ParameterName Returns or sets the name of the parameter
ParameterStatus Returns or sets the status of the parameter
ParameterValue Returns or sets the value of the parameter

Methods

Method Description
Dispose Dispose the spreadsheet object
GetValueList Get the list of values by giving a parameter name in spreadsheet
HasStatus Check if the parameter has the given status @return true or not

Enumerations

SpreadsheetDataParameterStatus Enumeration Represents the different spreadsheet parameter status

Property Detail

DescriptiveName

SpreadsheetDataParameter.DescriptiveName

Returns or sets the descriptive name of the parameter

-------------------------------------

Getter Method

Signature DescriptiveName()

Returns:descriptive name of the parameter
Return type:str

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DescriptiveName(descriptiveName)

Parameters:descriptiveName (str) – descriptive name of the parameter

New in version NX8.0.0.

License requirements: None.

ParameterName

SpreadsheetDataParameter.ParameterName

Returns or sets the name of the parameter

-------------------------------------

Getter Method

Signature ParameterName()

Returns:name of the parameter
Return type:str

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ParameterName(parameterName)

Parameters:parameterName (str) – name of the parameter

New in version NX8.0.0.

License requirements: None.

ParameterStatus

SpreadsheetDataParameter.ParameterStatus

Returns or sets the status of the parameter

-------------------------------------

Getter Method

Signature ParameterStatus()

Returns:status of the parameter
Return type:int

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ParameterStatus(parameterStatus)

Parameters:parameterStatus (int) – status of the parameter

New in version NX10.0.0.

License requirements: None.

ParameterValue

SpreadsheetDataParameter.ParameterValue

Returns or sets the value of the parameter

-------------------------------------

Getter Method

Signature ParameterValue()

Returns:value of the parameter
Return type:str

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ParameterValue(parameterValue)

Parameters:parameterValue (str) – value of the parameter

New in version NX8.0.0.

License requirements: None.

Method Detail

Dispose

SpreadsheetDataParameter.Dispose

Dispose the spreadsheet object

Signature Dispose()

New in version NX8.0.0.

License requirements: None.

GetValueList

SpreadsheetDataParameter.GetValueList

Get the list of values by giving a parameter name in spreadsheet

Signature GetValueList()

Returns:The list of values
Return type:list of str

New in version NX10.0.0.

License requirements: None.

HasStatus

SpreadsheetDataParameter.HasStatus

Check if the parameter has the given status

Signature HasStatus(parameterStatus)

Parameters:parameterStatus (NXOpen.Tooling.SpreadsheetDataParameterStatus) – status of the parameter
Returns:true or not
Return type:bool

New in version NX10.0.0.

License requirements: None.