SpreadsheetDataParameterStatus Enumeration

NXOpen.Tooling.SpreadsheetDataParameter.Status is an alias for NXOpen.Tooling.SpreadsheetDataParameterStatus

class NXOpen.Tooling.SpreadsheetDataParameterStatus

Bases: object

Represents the different spreadsheet parameter status

Enum Members

Enum Member Enum Member Description
Lock
User can’t change the value in UI
SystemKey
This is system key parameter
UserKey
Key parameter analyzed from spreadsheet search
HideStatus
Not shown in UI
ScaleItem
This is a scale item
ReadOnly
This parameter is read only
Modified
The parameter value is changed
ForceColor
If the parameter uses user value, normally it shows in UI in a different color. If this status is set, the parameter value will be shown in the same color.
HiddenValue
The parameter has value, but it should be hidden to user
OptionValue
The parameter has multiple value, but not treated as key parameter
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.