ProfileSplitBuilder Class¶
-
class
NXOpen.Tooling.
ProfileSplitBuilder
¶ Bases:
NXOpen.Builder
The ProfileSplit builder
To create a new instance of this class, use
NXOpen.Tooling.ProfileSplitCollection.CreateProfileSplitBuilder()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
DefAssociative | Returns or sets the associative flag |
DefVector | Returns or sets the extruded vector to return |
ExtDist1 | Returns the extruded start distance |
ExtDist2 | Returns the extruded end distance |
SelectBody | Returns the selected body to be splitted |
SelectProfile | Returns the selected profile |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
StTraverse | Start traverse function to get edge loop |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DefAssociative¶
-
ProfileSplitBuilder.
DefAssociative
¶ Returns or sets the associative flag
-------------------------------------
Getter Method
Signature
DefAssociative()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DefAssociative(defassociative)
Parameters: defassociative (bool) – New in version NX6.0.0.
License requirements: None.
DefVector¶
-
ProfileSplitBuilder.
DefVector
¶ Returns or sets the extruded vector to return
-------------------------------------
Getter Method
Signature
DefVector()
Returns: Return type: NXOpen.Direction
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DefVector(defVector)
Parameters: defVector ( NXOpen.Direction
) –New in version NX6.0.0.
License requirements: None.
ExtDist1¶
-
ProfileSplitBuilder.
ExtDist1
¶ Returns the extruded start distance
-------------------------------------
Getter Method
Signature
ExtDist1()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
ExtDist2¶
-
ProfileSplitBuilder.
ExtDist2
¶ Returns the extruded end distance
-------------------------------------
Getter Method
Signature
ExtDist2()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
SelectBody¶
-
ProfileSplitBuilder.
SelectBody
¶ Returns the selected body to be splitted
-------------------------------------
Getter Method
Signature
SelectBody()
Returns: Return type: NXOpen.SelectBodyList
New in version NX6.0.0.
License requirements: None.
SelectProfile¶
-
ProfileSplitBuilder.
SelectProfile
¶ Returns the selected profile
-------------------------------------
Getter Method
Signature
SelectProfile()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
Method Detail¶
StTraverse¶
-
ProfileSplitBuilder.
StTraverse
¶ Start traverse function to get edge loop
Signature
StTraverse()
New in version NX6.0.0.
License requirements: None.
Validate¶
-
ProfileSplitBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.