FlowAnalysisBuilder Class¶
-
class
NXOpen.Tooling.
FlowAnalysisBuilder
¶ Bases:
NXOpen.Builder
Represents the builder which is used to create flow analysis.
To create a new instance of this class, use
NXOpen.Tooling.MoldDesignCollection.CreateFlowAnalysisBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
Description | Returns or sets the size information of injection gates |
GatePoints | Returns the positions of injection gates |
ProductBody | Returns the product body |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Description¶
-
FlowAnalysisBuilder.
Description
¶ Returns or sets the size information of injection gates
-------------------------------------
Getter Method
Signature
Description()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Description(description)
Parameters: description (str) – New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”)
GatePoints¶
-
FlowAnalysisBuilder.
GatePoints
¶ Returns the positions of injection gates
-------------------------------------
Getter Method
Signature
GatePoints()
Returns: Return type: NXOpen.Section
New in version NX8.5.0.
License requirements: None.
ProductBody¶
-
FlowAnalysisBuilder.
ProductBody
¶ Returns the product body
-------------------------------------
Getter Method
Signature
ProductBody()
Returns: Return type: NXOpen.SelectBody
New in version NX8.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
FlowAnalysisBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.