CoolingPatternBuilder Class¶
-
class
NXOpen.Tooling.
CoolingPatternBuilder
¶ Bases:
NXOpen.Builder
The builder class for Cooling pattern which assists you to create channels with selected curves.
To create a new instance of this class, use
NXOpen.Tooling.CoolingPatternCollection.CreateCoolingPatternBuilder()
Default values.
Property Value Diameter.Value 10 (millimeters part), 0.375 (inches part) New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
ChannelDiameter | Returns or sets the channel diameter |
ChannelGuide | Returns the lines used to create the channel path. |
Diameter | Returns the channel diameter |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ChannelDiameter¶
-
CoolingPatternBuilder.
ChannelDiameter
¶ Returns or sets the channel diameter
-------------------------------------
Getter Method
Signature
ChannelDiameter()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ChannelDiameter(channelDiameter)
Parameters: channelDiameter (float) – New in version NX7.5.0.
License requirements: None.
ChannelGuide¶
-
CoolingPatternBuilder.
ChannelGuide
¶ Returns the lines used to create the channel path.
-------------------------------------
Getter Method
Signature
ChannelGuide()
Returns: Return type: NXOpen.Section
New in version NX7.5.0.
License requirements: None.
Diameter¶
-
CoolingPatternBuilder.
Diameter
¶ Returns the channel diameter
-------------------------------------
Getter Method
Signature
Diameter()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
CoolingPatternBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.