ConcurrentDesignManagementBuilder Class¶
-
class
NXOpen.Tooling.
ConcurrentDesignManagementBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Tooling.ConcurrentDesignManagementBuilder
to support concurrent design workflow management.To create a new instance of this class, use
NXOpen.Tooling.WorkflowManagementCollection.CreateConcurrentDesignManagementBuilder()
Default values.
Property Value SetAsMyDefaultTask 0 UpdateOptions SaveMyComponents New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
DesignTasks | Returns or sets the designer names. |
DesignerName | Returns or sets the designer name. |
ProjectLeader | Returns or sets the project leader name. |
SelectComponent | Returns the selected component to assign to a designer. |
SelectedDesignerIndex | Returns or sets the index of the selected designer. |
SetAsMyDefaultTask | Returns or sets the option to set as the current user’s default task. |
Tag | Returns the Tag for this object. |
TaskDescription | Returns or sets the task description string |
Type | Returns or sets the type of concurrent design management. |
UpdateOptions | Returns or sets the update type. |
UserName | Returns or sets the user name to login. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ConcurrentDesignManagementBuilderTypes Enumeration | Specifies the types of concurrent design management. |
ConcurrentDesignManagementBuilderUpdateTypes Enumeration | Specifies the types of the update action. |
Property Detail¶
DesignTasks¶
-
ConcurrentDesignManagementBuilder.
DesignTasks
¶ Returns or sets the designer names.
-------------------------------------
Getter Method
Signature
DesignTasks()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DesignTasks(designTasks)
Parameters: designTasks (str) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
DesignerName¶
-
ConcurrentDesignManagementBuilder.
DesignerName
¶ Returns or sets the designer name.
-------------------------------------
Getter Method
Signature
DesignerName()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DesignerName(designerName)
Parameters: designerName (str) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
ProjectLeader¶
-
ConcurrentDesignManagementBuilder.
ProjectLeader
¶ Returns or sets the project leader name.
-------------------------------------
Getter Method
Signature
ProjectLeader()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProjectLeader(projectLeader)
Parameters: projectLeader (str) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
SelectComponent¶
-
ConcurrentDesignManagementBuilder.
SelectComponent
¶ Returns the selected component to assign to a designer.
-------------------------------------
Getter Method
Signature
SelectComponent()
Returns: Return type: NXOpen.Assemblies.SelectComponent
New in version NX8.0.0.
License requirements: None.
SelectedDesignerIndex¶
-
ConcurrentDesignManagementBuilder.
SelectedDesignerIndex
¶ Returns or sets the index of the selected designer.
-------------------------------------
Getter Method
Signature
SelectedDesignerIndex()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectedDesignerIndex(selectedDesignerIndex)
Parameters: selectedDesignerIndex (int) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
SetAsMyDefaultTask¶
-
ConcurrentDesignManagementBuilder.
SetAsMyDefaultTask
¶ Returns or sets the option to set as the current user’s default task.
-------------------------------------
Getter Method
Signature
SetAsMyDefaultTask()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SetAsMyDefaultTask(setAsMyDefaultTask)
Parameters: setAsMyDefaultTask (bool) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
TaskDescription¶
-
ConcurrentDesignManagementBuilder.
TaskDescription
¶ Returns or sets the task description string
-------------------------------------
Getter Method
Signature
TaskDescription()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TaskDescription(taskDescription)
Parameters: taskDescription (str) – New in version NX10.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
Type¶
-
ConcurrentDesignManagementBuilder.
Type
¶ Returns or sets the type of concurrent design management.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Tooling.ConcurrentDesignManagementBuilderTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Tooling.ConcurrentDesignManagementBuilderTypes
) –New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
UpdateOptions¶
-
ConcurrentDesignManagementBuilder.
UpdateOptions
¶ Returns or sets the update type.
-------------------------------------
Getter Method
Signature
UpdateOptions()
Returns: Return type: NXOpen.Tooling.ConcurrentDesignManagementBuilderUpdateTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpdateOptions(updateOptions)
Parameters: updateOptions ( NXOpen.Tooling.ConcurrentDesignManagementBuilderUpdateTypes
) –New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
UserName¶
-
ConcurrentDesignManagementBuilder.
UserName
¶ Returns or sets the user name to login.
-------------------------------------
Getter Method
Signature
UserName()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserName(userName)
Parameters: userName (str) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
Method Detail¶
Validate¶
-
ConcurrentDesignManagementBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.