ConcurrentDesignManagementBuilderUpdateTypes Enumeration

NXOpen.Tooling.ConcurrentDesignManagementBuilder.UpdateTypes is an alias for NXOpen.Tooling.ConcurrentDesignManagementBuilderUpdateTypes

class NXOpen.Tooling.ConcurrentDesignManagementBuilderUpdateTypes

Bases: object

Specifies the types of the update action.

Enum Members

Enum Member Enum Member Description
SaveMyComponents
the save my components action
UpdateOtherComponents
the update other components action
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.