BomListBuilder Class¶
-
class
NXOpen.Tooling.
BomListBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Tooling.BomListBuilder
builder.To create a new instance of this class, use
NXOpen.Tooling.MoldwizardManager.CreateBomListBuilder()
Default values.
Property Value BomListType BomList New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
BomListDataProvider | Returns the data provider of BOM |
BomListType | Returns or sets the tree list shows which kind of components should be included in |
BomTemplate | Returns or sets the template file of bom |
SelectComponents | Returns the select component needed to get stocksize |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddBomData | Adds a new record into BOM list. |
Commit | Commits any edits that have been applied to the builder. |
CreatePartsList | Creates parts list for the assembly. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAttributeStrings | Gets all the attributes listed in the current template @return Attribute strings. |
GetColumn | Gets column number of given attribute |
GetColumnAttribute | Gets the corresponding attribute name of given column. |
GetColumnLabel | Gets the column label. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetPartOccs | Gets the corresponding part occurrences of given row. |
GetRows | Gets all the row numbers in the given List @return All row numbers in the given list |
IgnoreComponents | Ignores the corresponding components of given row in the Hide List so that the components can not be exported to spreadsheet. |
IgnoreRows | Ignores the given rows in the Hide List so that all the components of the rows can not be exported to spreadsheet. |
ModifyBomData | Modifies BOM data |
ParseBomTemplate | Parses the current BOM template. |
PopulateBomListData | Populates BOM list data according to current template. |
ShowComponents | Shows the corresponding components of given row in the BOM List so that the components can be exported to spreadsheet. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
ShowRows | Shows the given rows in the BOM List so that all the components of the rows can be exported to spreadsheet. |
SortColumn | Sorts the given column. |
UpdateEwBlankAttributes | Updates the blank attributes of electrodes in Electrode Design Application. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BomListBuilderBomListSortOption Enumeration | Represents an enumeration indicating whether the sorting needs to be performed in ascending or descending order. |
BomListBuilderBomListTypes Enumeration | Represents an index to components list type. |
Property Detail¶
BomListDataProvider¶
-
BomListBuilder.
BomListDataProvider
¶ Returns the data provider of BOM
-------------------------------------
Getter Method
Signature
BomListDataProvider()
Returns: Return type: NXOpen.Tooling.BomListDataProvider
New in version NX11.0.0.
License requirements: None.
BomListType¶
-
BomListBuilder.
BomListType
¶ Returns or sets the tree list shows which kind of components should be included in
-------------------------------------
Getter Method
Signature
BomListType()
Returns: Return type: NXOpen.Tooling.BomListBuilderBomListTypes
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BomListType(bomListType)
Parameters: bomListType ( NXOpen.Tooling.BomListBuilderBomListTypes
) –New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
BomTemplate¶
-
BomListBuilder.
BomTemplate
¶ Returns or sets the template file of bom
-------------------------------------
Getter Method
Signature
BomTemplate()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BomTemplate(bomTemplate)
Parameters: bomTemplate (str) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SelectComponents¶
-
BomListBuilder.
SelectComponents
¶ Returns the select component needed to get stocksize
-------------------------------------
Getter Method
Signature
SelectComponents()
Returns: Return type: NXOpen.Assemblies.SelectComponentList
New in version NX10.0.0.
License requirements: None.
Method Detail¶
AddBomData¶
-
BomListBuilder.
AddBomData
¶ Adds a new record into BOM list.
Signature
AddBomData(partOccs, dataStrings)
Parameters: - partOccs (list of
NXOpen.Assemblies.Component
) – The part occurrences to add into BOM. Sets NULL to add the current display part into BOM list. - dataStrings (list of str) – The BOM data.
New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
- partOccs (list of
CreatePartsList¶
-
BomListBuilder.
CreatePartsList
¶ Creates parts list for the assembly.
Signature
CreatePartsList(columnWidths, point)
Parameters: - columnWidths (list of int) – The widths of each column.
- point (
NXOpen.Point3d
) – The position of parts list.
Returns: The created parts list.
Return type: New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
GetAttributeStrings¶
-
BomListBuilder.
GetAttributeStrings
¶ Gets all the attributes listed in the current template
Signature
GetAttributeStrings()
Returns: Attribute strings. Return type: list of str New in version NX10.0.0.
Deprecated since version NX11.0.0: Use
Tooling.BomListBuilder.GetColumnAttribute()
instead.License requirements: None.
GetColumn¶
-
BomListBuilder.
GetColumn
¶ Gets column number of given attribute
Signature
GetColumn(attrString)
Parameters: attrString (str) – New in version NX10.0.0.
Deprecated since version NX11.0.0: Use
Tooling.BomListBuilder.GetColumnAttribute()
instead.License requirements: None.
GetColumnAttribute¶
-
BomListBuilder.
GetColumnAttribute
¶ Gets the corresponding attribute name of given column.
Signature
GetColumnAttribute(columnID)
Parameters: columnID (int) – Column index Returns: Column attribute Return type: str New in version NX11.0.0.
License requirements: None.
GetColumnLabel¶
-
BomListBuilder.
GetColumnLabel
¶ Gets the column label.
Signature
GetColumnLabel(columnID)
Parameters: columnID (int) – Column index Returns: Column Label Return type: str New in version NX11.0.0.
License requirements: None.
GetPartOccs¶
-
BomListBuilder.
GetPartOccs
¶ Gets the corresponding part occurrences of given row.
Signature
GetPartOccs(rowID)
Parameters: rowID (int) – Returns: The corresponding part occurrences of given row. Return type: list of NXOpen.Assemblies.Component
New in version NX10.0.0.
License requirements: None.
GetRows¶
-
BomListBuilder.
GetRows
¶ Gets all the row numbers in the given List
Signature
GetRows(bomListType)
Parameters: bomListType ( NXOpen.Tooling.BomListBuilderBomListTypes
) –Returns: All row numbers in the given list Return type: list of int New in version NX10.0.0.
Deprecated since version NX11.0.0: Use
Tooling.BomListDataProvider.RowCount()
instead.License requirements: None.
IgnoreComponents¶
-
BomListBuilder.
IgnoreComponents
¶ Ignores the corresponding components of given row in the Hide List so that the components can not be exported to spreadsheet.
Signature
IgnoreComponents(rowID, partOccs)
Parameters: - rowID (int) –
- partOccs (list of
NXOpen.Assemblies.Component
) – The part occurrences to be ignored in Hide List. Sets NULL to ignore all part occurrences in given row in Hide List.
New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
IgnoreRows¶
-
BomListBuilder.
IgnoreRows
¶ Ignores the given rows in the Hide List so that all the components of the rows can not be exported to spreadsheet.
Signature
IgnoreRows(rowIDs)
Parameters: rowIDs (list of int) – New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
ModifyBomData¶
-
BomListBuilder.
ModifyBomData
¶ Modifies BOM data
Signature
ModifyBomData(rowNumber, columnNumber, userString)
Parameters: - rowNumber (int) –
- columnNumber (int) –
- userString (str) –
New in version NX10.0.0.
Deprecated since version NX11.0.0: Use
Tooling.BomListDataProvider.SetString()
instead.License requirements: None.
ParseBomTemplate¶
-
BomListBuilder.
ParseBomTemplate
¶ Parses the current BOM template.
Use this function to populate data in data provider of BOM.
Signature
ParseBomTemplate()
New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
PopulateBomListData¶
-
BomListBuilder.
PopulateBomListData
¶ Populates BOM list data according to current template.
Signature
PopulateBomListData()
New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
ShowComponents¶
-
BomListBuilder.
ShowComponents
¶ Shows the corresponding components of given row in the BOM List so that the components can be exported to spreadsheet.
Signature
ShowComponents(rowID, partOccs)
Parameters: - rowID (int) –
- partOccs (list of
NXOpen.Assemblies.Component
) – The part occurrences to be shown in BOM List. Sets NULL show all part occurrences in given row in BOM List.
New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
ShowRows¶
-
BomListBuilder.
ShowRows
¶ Shows the given rows in the BOM List so that all the components of the rows can be exported to spreadsheet.
Signature
ShowRows(rowIDs)
Parameters: rowIDs (list of int) – New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SortColumn¶
-
BomListBuilder.
SortColumn
¶ Sorts the given column.
Signature
SortColumn(columnID, order)
Parameters: - columnID (int) –
- order (
NXOpen.Tooling.BomListBuilderBomListSortOption
) –
New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
UpdateEwBlankAttributes¶
-
BomListBuilder.
UpdateEwBlankAttributes
¶ Updates the blank attributes of electrodes in Electrode Design Application.
Signature
UpdateEwBlankAttributes()
New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Validate¶
-
BomListBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.