BomListBuilderBomListSortOption Enumeration¶
NXOpen.Tooling.BomListBuilder.BomListSortOption is an alias for NXOpen.Tooling.BomListBuilderBomListSortOption
-
class
NXOpen.Tooling.
BomListBuilderBomListSortOption
¶ Bases:
object
Represents an enumeration indicating whether the sorting needs to be performed in ascending or descending order.
Enum Members
Enum Member Enum Member Description Unsorted UnsortedAscending AscendingDescending Descending-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-