SessionMeasureRequirements Class¶
-
class
NXOpen.Preferences.
SessionMeasureRequirements
¶ Bases:
object
Represents the two options available on the Measure Requirements toolbar and applicable to the entire session
To obtain an instance of this class, refer to
NXOpen.Preferences.SessionPreferences
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
UpdateFrameRate | Returns or sets the frame rate. |
ViolationAction | Returns or sets the violation action. |
Methods¶
Enumerations¶
SessionMeasureRequirementsActionOnViolation Enumeration | Values for the action to take when a requirement error is generated for a measure with a displayed annotation in Assembly Sequencing. |
Property Detail¶
UpdateFrameRate¶
-
SessionMeasureRequirements.
UpdateFrameRate
¶ Returns or sets the frame rate.
The frame rate specifies how frequently a displayed measure annotation is updated in Assembly Sequencing. So a rate of 1 specifies that the annotation will update every frame during playback. A rate of 5 specifies that the annotation will update every fifth frame during playback.
-------------------------------------
Getter Method
Signature
UpdateFrameRate()
Returns: an integer <ja_gt> 0 Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpdateFrameRate(frameRate)
Parameters: frameRate (int) – an integer <ja_gt> 0 New in version NX5.0.0.
License requirements: None.
ViolationAction¶
-
SessionMeasureRequirements.
ViolationAction
¶ Returns or sets the violation action.
The violation action is one of the enumerated type values.
-------------------------------------
Getter Method
Signature
ViolationAction()
Returns: Return type: NXOpen.Preferences.SessionMeasureRequirementsActionOnViolation
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ViolationAction(violationAction)
Parameters: violationAction ( NXOpen.Preferences.SessionMeasureRequirementsActionOnViolation
) –New in version NX5.0.0.
License requirements: None.