SessionMeasureRequirementsActionOnViolation Enumeration

NXOpen.Preferences.SessionMeasureRequirements.ActionOnViolation is an alias for NXOpen.Preferences.SessionMeasureRequirementsActionOnViolation

class NXOpen.Preferences.SessionMeasureRequirementsActionOnViolation

Bases: object

Values for the action to take when a requirement error is generated for a measure with a displayed annotation in Assembly Sequencing.

Enum Members

Enum Member Enum Member Description
HightlightMeasure
Highlight (color) measure for requirements violations
StopPlayback
Suspend playback and wait for acknowledgement for requirements violations
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.