PartVisualizationLine Class

class NXOpen.Preferences.PartVisualizationLine

Bases: object

Represents the set of visualization preferences under Line tab applicable to part

To obtain an instance of this class, refer to NXOpen.Preferences.PartPreferences

New in version NX3.0.0.

Properties

Property Description
CurveTolerance Returns or sets the curve tolerance.
DashSize Returns or sets the dash size.
LineFontDisplay Returns or sets the line font display.
ShowWidths Returns or sets the show widths option.
SpaceSize Returns or sets the space size.
SymbolSize Returns or sets the symbol size.
WidthScale Returns or sets the width scale option.

Methods

Method Description
GetPixelWidthOptions Returns pixel widths used in the graphics window.
GetPixelWidths Returns options that control width appearance in the graphics window.
GetWidthOptions Returns the show widths and width scale options.
ResetPixelWidthOptions Resets all pixel width options to settings specified by customer defaults.
SetPixelWidthOptions Modifies options that control width appearance in the graphics window.
SetPixelWidths Modifies pixel widths used in the graphics window.
SetWidthOptions Modifies the show widths and width scale options.

Enumerations

PartVisualizationLineLineFontDisplayType Enumeration Describes whether Line Font Display type is hardware or software.

Property Detail

CurveTolerance

PartVisualizationLine.CurveTolerance

Returns or sets the curve tolerance.

Specifies the level of detail for the current Display Mode.

-------------------------------------

Getter Method

Signature CurveTolerance()

Returns:
Return type:float

New in version NX3.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CurveTolerance(lineCurveTolerance)

Parameters:lineCurveTolerance (float) –

New in version NX3.0.0.

License requirements: None.

DashSize

PartVisualizationLine.DashSize

Returns or sets the dash size.

Sets the length of a segment of a dashed curve.

-------------------------------------

Getter Method

Signature DashSize()

Returns:
Return type:float

New in version NX3.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DashSize(lineDashSize)

Parameters:lineDashSize (float) –

New in version NX3.0.0.

License requirements: None.

LineFontDisplay

PartVisualizationLine.LineFontDisplay

Returns or sets the line font display.

Controls the line font. The Hardware option uses the system graphics library to generate the seven standard line fonts. Selecting hardware line fonts can improve drawing performance and reduce memory consumption. The Software option generates non-solid curves with the values entered for the Dash, Space, and Symbol size.

-------------------------------------

Getter Method

Signature LineFontDisplay()

Returns:
Return type:NXOpen.Preferences.PartVisualizationLineLineFontDisplayType

New in version NX3.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature LineFontDisplay(lineFontDisplay)

Parameters:lineFontDisplay (NXOpen.Preferences.PartVisualizationLineLineFontDisplayType) –

New in version NX3.0.0.

License requirements: None.

ShowWidths

PartVisualizationLine.ShowWidths

Returns or sets the show widths option.

If true, the object width attribute determines the displayed width of lines or curves used to represent an object.If false, all curves are drawn thin, regardless of object width settings.

-------------------------------------

Getter Method

Signature ShowWidths()

Returns:
Return type:bool

New in version NX3.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ShowWidths(isShowWidthOn)

Parameters:isShowWidthOn (bool) –

New in version NX3.0.0.

License requirements: None.

SpaceSize

PartVisualizationLine.SpaceSize

Returns or sets the space size.

Sets the distance between two segments of a dashed curve.

-------------------------------------

Getter Method

Signature SpaceSize()

Returns:
Return type:float

New in version NX3.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SpaceSize(lineSpaceSize)

Parameters:lineSpaceSize (float) –

New in version NX3.0.0.

License requirements: None.

SymbolSize

PartVisualizationLine.SymbolSize

Returns or sets the symbol size.

Controls the displayed size of symbols used in software line fonts.

-------------------------------------

Getter Method

Signature SymbolSize()

Returns:
Return type:float

New in version NX3.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SymbolSize(lineSymbolSize)

Parameters:lineSymbolSize (float) –

New in version NX3.0.0.

License requirements: None.

WidthScale

PartVisualizationLine.WidthScale

Returns or sets the width scale option.

Controls scaling of the width of lines and curves displayed in the graphics window. If set to 0.0 (the minimum value), widths range from 1 to 3 pixels. If set to 1.0 (the maximum value), widths range from 1 to the maximum supported pixel width.

-------------------------------------

Getter Method

Signature WidthScale()

Returns:
Return type:float

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature WidthScale(widthScale)

Parameters:widthScale (float) –

New in version NX8.5.0.

License requirements: None.

Method Detail

GetPixelWidthOptions

PartVisualizationLine.GetPixelWidthOptions

Returns pixel widths used in the graphics window.

Signature GetPixelWidthOptions()

Returns:a tuple
Return type:A tuple consisting of (useWidthScale, widthScale, pixelWidths). useWidthScale is a bool. If true, width appearance in the graphics window is controlled by width scale. If false, width appearance is controlled by pixel widths. widthScale is a float. the width scale option, which controls scaling of widths in the graphics window when useWidthScale is true. If set to 0.0 (the minimum value), widths range from 1 to 3 pixels. If set to 1.0 (the maximum value), widths range from 1 to 9 pixels. pixelWidths is a list of int. Array of 9 pixel widths, one for each of the 9 width settings, that defines the appearance of widths in the graphics window when useWidthScale is false. Valid pixel widths range from 1 to 9.

New in version NX10.0.0.

License requirements: None.

GetPixelWidths

PartVisualizationLine.GetPixelWidths

Returns options that control width appearance in the graphics window.

Signature GetPixelWidths()

Returns:

Array of 9 pixel widths, one for each of the 9 width settings, that defines the appearance of widths in the graphics window. Valid pixel widths range from 1 to 9. :rtype: list of int

New in version NX10.0.0.

License requirements: None.

GetWidthOptions

PartVisualizationLine.GetWidthOptions

Returns the show widths and width scale options.

Signature GetWidthOptions()

Returns:a tuple
Return type:A tuple consisting of (showWidths, widthScale). showWidths is a bool. the show widths option, which controls whether or not the object width attribute determines the displayed width of lines and curves. widthScale is a float. the width scale option, which controls scaling of the width of lines and curves displayed in the graphics window.

New in version NX8.5.0.

License requirements: None.

ResetPixelWidthOptions

PartVisualizationLine.ResetPixelWidthOptions

Resets all pixel width options to settings specified by customer defaults.

Signature ResetPixelWidthOptions()

New in version NX10.0.0.

License requirements: None.

SetPixelWidthOptions

PartVisualizationLine.SetPixelWidthOptions

Modifies options that control width appearance in the graphics window.

Signature SetPixelWidthOptions(useWidthScale, widthScale, pixelWidths)

Parameters:
  • useWidthScale (bool) – If true, width appearance in the graphics window is controlled by width scale. If false, width appearance is controlled by pixel widths.
  • widthScale (float) – the width scale option, which controls scaling of widths in the graphics window when useWidthScale is true. If set to 0.0 (the minimum value), widths range from 1 to 3 pixels. If set to 1.0 (the maximum value), widths range from 1 to 9 pixels.
  • pixelWidths (list of int) – Array of 9 pixel widths, one for each of the 9 width settings, that defines the appearance of widths in the graphics window when useWidthScale is false. Valid pixel widths range from 1 to 9.

New in version NX10.0.0.

License requirements: None.

SetPixelWidths

PartVisualizationLine.SetPixelWidths

Modifies pixel widths used in the graphics window.

Signature SetPixelWidths(pixelWidths)

Parameters:pixelWidths (list of int) – Array of 9 pixel widths, one for each of the 9 width settings, that defines the appearance of widths in the graphics window. Valid pixel widths range from 1 to 9.

New in version NX10.0.0.

License requirements: None.

SetWidthOptions

PartVisualizationLine.SetWidthOptions

Modifies the show widths and width scale options.

Signature SetWidthOptions(showWidths, widthScale)

Parameters:
  • showWidths (bool) – the show widths option, which controls whether or not the object width attribute determines the displayed width of lines and curves.
  • widthScale (float) – the width scale option, which controls scaling of the width of lines and curves displayed in the graphics window.

New in version NX8.5.0.

License requirements: None.