PartVisualizationLineLineFontDisplayType Enumeration

NXOpen.Preferences.PartVisualizationLine.LineFontDisplayType is an alias for NXOpen.Preferences.PartVisualizationLineLineFontDisplayType

class NXOpen.Preferences.PartVisualizationLineLineFontDisplayType

Bases: object

Describes whether Line Font Display type is hardware or software.

Enum Members

Enum Member Enum Member Description
Software  
Hardware  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.