TextDocumentData Class¶
-
class
NXOpen.OpenXml.
TextDocumentData
¶ Bases:
NXOpen.OpenXml.DocumentData
Represents the text to be exported to the speific Open XML file.
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetContent | Gets the content to be exported of text data @return |
GetDataType | Gets a specified document data type @return the data type defined by the NXOpen.OpenXml.DocumentDataType |
SetContent | Sets the content to be exported of text data |
Method Detail¶
Dispose¶
-
TextDocumentData.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.