DocumentData Class¶
-
class
NXOpen.OpenXml.
DocumentData
¶ Bases:
NXOpen.TransientObject
Represents the definition of the base document data
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetDataType | Gets a specified document data type @return the data type defined by the NXOpen.OpenXml.DocumentDataType |
Enumerations¶
DocumentDataType Enumeration | the document data type |
Method Detail¶
Dispose¶
-
DocumentData.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
GetDataType¶
-
DocumentData.
GetDataType
¶ Gets a specified document data type
Signature
GetDataType()
Returns: the data type defined by the NXOpen.OpenXml.DocumentDataType
Return type: NXOpen.OpenXml.DocumentDataType
New in version NX11.0.0.
License requirements: None.