TableDocumentData Class¶
-
class
NXOpen.OpenXml.
TableDocumentData
¶ Bases:
NXOpen.OpenXml.DocumentData
Represents the table to be exported to the speific Open XML file.
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
AddCellData | Creates a new NXOpen.OpenXml.TableCellData object. |
Dispose | Frees the object from memory. |
GetCaption | Gets the caption of the table data @return |
GetCellsCount | Gets the number of table cells @return number of table cells |
GetColumnCount | Gets the column count of table data @return |
GetColumnWidths | Gets the width array of the columns @return the column width array |
GetDataType | Gets a specified document data type @return the data type defined by the NXOpen.OpenXml.DocumentDataType |
GetNthCell | Gets the nth table cell data @return the table cell data |
GetRowCount | Gets the row count of table data @return |
GetRowHeigths | Gets the height array of the rows @return the column width array |
SetCaption | Sets the caption of the table data |
SetColumnWidths | Sets the width array of the columns |
SetRowHeigths | Sets the height array of the rows |
Enumerations¶
TableDocumentDataCaptionPosition Enumeration | the location of the caption for table data |
Method Detail¶
AddCellData¶
-
TableDocumentData.
AddCellData
¶ Creates a new
NXOpen.OpenXml.TableCellData
object.Does not to free this object, it will be free while deleting
NXOpen.OpenXml.TableDocumentData
objectSignature
AddCellData(grids)
Parameters: grids (list of int) – the grid IDs to be mergered into the cell data Returns: the table cell data Return type: NXOpen.OpenXml.TableCellData
New in version NX11.0.0.
License requirements: None.
Dispose¶
-
TableDocumentData.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
GetCellsCount¶
-
TableDocumentData.
GetCellsCount
¶ Gets the number of table cells
Signature
GetCellsCount()
Returns: number of table cells Return type: int New in version NX11.0.0.
License requirements: None.
GetColumnCount¶
-
TableDocumentData.
GetColumnCount
¶ Gets the column count of table data
Signature
GetColumnCount()
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
GetColumnWidths¶
-
TableDocumentData.
GetColumnWidths
¶ Gets the width array of the columns
Signature
GetColumnWidths()
Returns: the column width array Return type: list of float New in version NX11.0.0.
License requirements: None.
GetNthCell¶
-
TableDocumentData.
GetNthCell
¶ Gets the nth table cell data
Signature
GetNthCell(index)
Parameters: index (int) – the index of table cell data Returns: the table cell data Return type: NXOpen.OpenXml.TableCellData
New in version NX11.0.0.
License requirements: None.
GetRowCount¶
-
TableDocumentData.
GetRowCount
¶ Gets the row count of table data
Signature
GetRowCount()
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
GetRowHeigths¶
-
TableDocumentData.
GetRowHeigths
¶ Gets the height array of the rows
Signature
GetRowHeigths()
Returns: the column width array Return type: list of float New in version NX11.0.0.
License requirements: None.