TireCollection Class¶
-
class
NXOpen.Motion.
TireCollection
¶ Bases:
object
Represents a collection of motion tire elements
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateTireBuilder | Return NXOpen.Motion.TireBuilder object @return TireBuilder object |
FindObject | Finds the NXOpen.Motion.Tire with the given name. |
Method Detail¶
CreateTireBuilder¶
-
TireCollection.
CreateTireBuilder
¶ Return
NXOpen.Motion.TireBuilder
objectSignature
CreateTireBuilder(tire)
Parameters: tire ( NXOpen.Motion.Tire
) –NXOpen.Motion.TireBuilder
to be edited, if None then create a new oneReturns: TireBuilder object Return type: NXOpen.Motion.TireBuilder
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
TireCollection.
FindObject
¶ Finds the
NXOpen.Motion.Tire
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – the object name Returns: the object pointer Return type: NXOpen.Motion.Tire
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)