TireBuilder Class¶
-
class
NXOpen.Motion.
TireBuilder
¶ Bases:
NXOpen.Motion.MotionBuilder
Represents a
Motion.Tire
builderTo create a new instance of this class, use
NXOpen.Motion.TireCollection.CreateTireBuilder()
Default values.
Property Value DisplayScale 1.0 TireType Basic New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
BodyLink | Returns the body link. |
BodyPoint | Returns or sets the body point. |
BodyVector | Returns or sets the body vector. |
CarrierCsys | Returns or sets the carrier coordinate system. |
CarrierLink | Returns the carrier link. |
CarrierPoint | Returns or sets the carrier point. |
ChassisCsys | Returns or sets the chassis coordinate system. |
ChassisLink | Returns the chassis link. |
ChassisPoint | Returns or sets the chassis point. |
DisplayScale | Returns or sets the icon display scale |
GroupName | Returns or sets the group name |
GroupType | Returns or sets the group type |
Name | Returns or sets the unique name assigned to the tire component |
PropertyBasic | Returns the basic tire property. |
PropertyCd | Returns the CD tire property. |
PropertyFTire | Returns the FT tire property. |
PropertyMotorcycle | Returns the motorcycle tire property. |
PropertyNonInertial | Returns the non-inertial tire property. |
PropertyTno | Returns the TNO tire property. |
Road | Returns the road. |
Tag | Returns the Tag for this object. |
TireType | Returns or sets the tire type. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TireBuilderType Enumeration | the Tire type. |
Property Detail¶
BodyLink¶
-
TireBuilder.
BodyLink
¶ Returns the body link.
This is a link defining the Tire body.
-------------------------------------
Getter Method
Signature
BodyLink()
Returns: Return type: NXOpen.Motion.SelectLink
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
BodyPoint¶
-
TireBuilder.
BodyPoint
¶ Returns or sets the body point.
This represents the center of the wheel.
-------------------------------------
Getter Method
Signature
BodyPoint()
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
BodyPoint(bodyPoint)
Parameters: bodyPoint ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
BodyVector¶
-
TireBuilder.
BodyVector
¶ Returns or sets the body vector.
This defines the spinning direction.
-------------------------------------
Getter Method
Signature
BodyVector()
Returns: Return type: NXOpen.Direction
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
BodyVector(bodyVector)
Parameters: bodyVector ( NXOpen.Direction
) –New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
CarrierCsys¶
-
TireBuilder.
CarrierCsys
¶ Returns or sets the carrier coordinate system.
This represents a coordinate systeme attached to the chassis for which: z axis defines the up direction and the x axis defines the forward direction of the chassis. It is only used by external tires.
-------------------------------------
Getter Method
Signature
CarrierCsys()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
CarrierCsys(csys)
Parameters: csys ( NXOpen.CoordinateSystem
) –New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
CarrierLink¶
-
TireBuilder.
CarrierLink
¶ Returns the carrier link.
This represents the link where the tire will be attached. It is only used by external tires.
-------------------------------------
Getter Method
Signature
CarrierLink()
Returns: Return type: NXOpen.Motion.SelectLink
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
CarrierPoint¶
-
TireBuilder.
CarrierPoint
¶ Returns or sets the carrier point.
This represents the attachment point of the tire link on the chassis link. It is only used by external tires.
-------------------------------------
Getter Method
Signature
CarrierPoint()
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
CarrierPoint(point)
Parameters: point ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
ChassisCsys¶
-
TireBuilder.
ChassisCsys
¶ Returns or sets the chassis coordinate system.
This represents a coordinate systeme attached to the chassis for which z axis defines the up direction and the x axis defines the forward direction of the chassis. For external tires it is optional and it is used for the purposes of including additional stabilizing stiffness to the vehicle link during static analysis, provided that the Static Hold variable is TRUE. Ideally all tire elements should refer to the same Chassis axis system. If this optional parameter is not defined, the stabilizing stiffness will be applied to the selected axis system on the carrier link. This approach may introduce unwanted transients into a STATIC/DYNAMIC simulation.
-------------------------------------
Getter Method
Signature
ChassisCsys()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
ChassisCsys(chassisCsys)
Parameters: chassisCsys ( NXOpen.CoordinateSystem
) –New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
ChassisLink¶
-
TireBuilder.
ChassisLink
¶ Returns the chassis link.
This represents the link where the tire will be attached. For external tires it is used for static data analysis.
-------------------------------------
Getter Method
Signature
ChassisLink()
Returns: Return type: NXOpen.Motion.SelectLink
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
ChassisPoint¶
-
TireBuilder.
ChassisPoint
¶ Returns or sets the chassis point.
This represents the attachment point of the tire body on the chassis link.
-------------------------------------
Getter Method
Signature
ChassisPoint()
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
ChassisPoint(chassisPoint)
Parameters: chassisPoint ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
Name¶
-
TireBuilder.
Name
¶ Returns or sets the unique name assigned to the tire component
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
PropertyBasic¶
-
TireBuilder.
PropertyBasic
¶ Returns the basic tire property.
This is an object used to hold parameters for Basic tire type.
-------------------------------------
Getter Method
Signature
PropertyBasic()
Returns: Return type: NXOpen.Motion.SelectTirePropertyBasic
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
PropertyCd¶
-
TireBuilder.
PropertyCd
¶ Returns the CD tire property.
This is an object used to hold parameters for CDTire type
-------------------------------------
Getter Method
Signature
PropertyCd()
Returns: Return type: NXOpen.Motion.SelectTirePropertyCd
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
PropertyFTire¶
-
TireBuilder.
PropertyFTire
¶ Returns the FT tire property.
This is an object used to hold parameters for FTire type
-------------------------------------
Getter Method
Signature
PropertyFTire()
Returns: Return type: NXOpen.Motion.SelectTirePropertyFt
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
PropertyMotorcycle¶
-
TireBuilder.
PropertyMotorcycle
¶ Returns the motorcycle tire property.
This is an object used to hold parameters for Motorcycle tire type.
-------------------------------------
Getter Method
Signature
PropertyMotorcycle()
Returns: Return type: NXOpen.Motion.SelectTirePropertyMotorcycle
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
PropertyNonInertial¶
-
TireBuilder.
PropertyNonInertial
¶ Returns the non-inertial tire property.
This is an object used to hold parameters for Non-Inertial tire type.
-------------------------------------
Getter Method
Signature
PropertyNonInertial()
Returns: Return type: NXOpen.Motion.SelectTirePropertyNonInertial
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
PropertyTno¶
-
TireBuilder.
PropertyTno
¶ Returns the TNO tire property.
This is an object used to hold parameters for TNO Tire type
-------------------------------------
Getter Method
Signature
PropertyTno()
Returns: Return type: NXOpen.Motion.SelectTirePropertyTno
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
Road¶
-
TireBuilder.
Road
¶ Returns the road.
This parameter defines the road height Z and slope of the road surface depending on the X and Y location of the tire. If no road is selected, the road profile will default to the global XY plane.
-------------------------------------
Getter Method
Signature
Road()
Returns: Return type: NXOpen.Motion.SelectRoad
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
TireType¶
-
TireBuilder.
TireType
¶ Returns or sets the tire type.
Defines the type of the tire used, different tire types use different parameters
-------------------------------------
Getter Method
Signature
TireType()
Returns: Return type: NXOpen.Motion.TireBuilderType
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
TireType(typeSelection)
Parameters: typeSelection ( NXOpen.Motion.TireBuilderType
) –New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
Validate¶
-
TireBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.