SignalChartCollection Class¶
-
class
NXOpen.Motion.
SignalChartCollection
¶ Bases:
object
Represents a collection of motion Signal Chart
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreateSignalChartBuilder | Return NXOpen.Motion.SignalChartBuilder object @return SignalChartBuilder object |
CreateSignalChartListItem | Creates a NXOpen.Motion.SignalChartListItem @return |
FindObject | Finds the NXOpen.Motion.SignalChart with the given name. |
Method Detail¶
CreateSignalChartBuilder¶
-
SignalChartCollection.
CreateSignalChartBuilder
¶ Return
NXOpen.Motion.SignalChartBuilder
objectSignature
CreateSignalChartBuilder(signalchart)
Parameters: signalchart ( NXOpen.Motion.SignalChart
) –NXOpen.Motion.SignalChart
to be edited, if None then create a new oneReturns: SignalChartBuilder object Return type: NXOpen.Motion.SignalChartBuilder
New in version NX6.0.0.
License requirements: nx_motion_motor (“NX Motion Motor”)
CreateSignalChartListItem¶
-
SignalChartCollection.
CreateSignalChartListItem
¶ Creates a
NXOpen.Motion.SignalChartListItem
Signature
CreateSignalChartListItem()
Returns: Return type: NXOpen.Motion.SignalChartListItem
New in version NX6.0.0.
License requirements: nx_motion_motor (“NX Motion Motor”)
FindObject¶
-
SignalChartCollection.
FindObject
¶ Finds the
NXOpen.Motion.SignalChart
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – Returns: Return type: NXOpen.Motion.SignalChart
New in version NX6.0.0.
License requirements: nx_motion_motor (“NX Motion Motor”)