SignalChartBuilder Class¶
-
class
NXOpen.Motion.
SignalChartBuilder
¶ Bases:
NXOpen.Motion.MotionBuilder
Represents a
NXOpen.Motion.SignalChartBuilder
To create a new instance of this class, use
NXOpen.Motion.SignalChartCollection.CreateSignalChartBuilder()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ClosedSignalList | Returns the closed siganl list |
DisplayScale | Returns or sets the icon display scale |
GroupName | Returns or sets the group name |
GroupType | Returns or sets the group type |
InitialSignal | Returns or sets the initial Signal |
InitialSignalExpression | Returns the initial Signal Expression |
Name | Returns or sets the name |
OpenSignalFunction | Returns or sets the open signal function |
SignalChartType | Returns or sets the SignalChart type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
NewListItem | Creates a new list item @return |
NewListItemExpression | Creates a new list item including expression @return |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SignalChartBuilderType Enumeration | SignalChart type |
Property Detail¶
ClosedSignalList¶
-
SignalChartBuilder.
ClosedSignalList
¶ Returns the closed siganl list
-------------------------------------
Getter Method
Signature
ClosedSignalList()
Returns: Return type: NXOpen.Motion.SignalChartListItemList
New in version NX6.0.0.
License requirements: nx_motion_motor (“NX Motion Motor”)
InitialSignal¶
-
SignalChartBuilder.
InitialSignal
¶ Returns or sets the initial Signal
-------------------------------------
Getter Method
Signature
InitialSignal()
Returns: Return type: float New in version NX6.0.0.
Deprecated since version NX8.5.0: Obtain the expression using
NXOpen.Motion.SignalChartBuilder.InitialSignalExpression()
to query or edit it.License requirements: nx_motion_motor (“NX Motion Motor”)
-------------------------------------
Setter Method
Signature
InitialSignal(initialSignal)
Parameters: initialSignal (float) – New in version NX6.0.0.
Deprecated since version NX8.5.0: Obtain the expression using
NXOpen.Motion.SignalChartBuilder.InitialSignalExpression()
to query or edit it.License requirements: nx_motion_motor (“NX Motion Motor”)
InitialSignalExpression¶
-
SignalChartBuilder.
InitialSignalExpression
¶ Returns the initial Signal Expression
-------------------------------------
Getter Method
Signature
InitialSignalExpression()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: nx_motion_motor (“NX Motion Motor”)
Name¶
-
SignalChartBuilder.
Name
¶ Returns or sets the name
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX6.0.0.
License requirements: nx_motion_motor (“NX Motion Motor”)
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX6.0.0.
License requirements: nx_motion_motor (“NX Motion Motor”)
OpenSignalFunction¶
-
SignalChartBuilder.
OpenSignalFunction
¶ Returns or sets the open signal function
-------------------------------------
Getter Method
Signature
OpenSignalFunction()
Returns: Return type: NXOpen.CAE.Function
New in version NX6.0.0.
License requirements: nx_motion_motor (“NX Motion Motor”)
-------------------------------------
Setter Method
Signature
OpenSignalFunction(openSignalFunction)
Parameters: openSignalFunction ( NXOpen.CAE.Function
) –New in version NX6.0.0.
License requirements: nx_motion_motor (“NX Motion Motor”)
SignalChartType¶
-
SignalChartBuilder.
SignalChartType
¶ Returns or sets the SignalChart type
-------------------------------------
Getter Method
Signature
SignalChartType()
Returns: Return type: NXOpen.Motion.SignalChartBuilderType
New in version NX6.0.0.
License requirements: nx_motion_motor (“NX Motion Motor”)
-------------------------------------
Setter Method
Signature
SignalChartType(signalchartType)
Parameters: signalchartType ( NXOpen.Motion.SignalChartBuilderType
) –New in version NX6.0.0.
License requirements: nx_motion_motor (“NX Motion Motor”)
Method Detail¶
NewListItem¶
-
SignalChartBuilder.
NewListItem
¶ Creates a new list item
Signature
NewListItem(sensor, alwaysEvaluated, timeSensor, condition, threshold, delayTime, signal)
Parameters: - sensor (
NXOpen.Motion.MotionSensor
) – sensor - alwaysEvaluated (bool) – always evaluted
- timeSensor (int) – time sensor
- condition (int) – condition
- threshold (float) – threshold
- delayTime (float) – delay time
- signal (float) – signal
Returns: Return type: New in version NX6.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Motion.SignalChartBuilder.NewListItemExpression()
instead.License requirements: nx_motion_motor (“NX Motion Motor”)
- sensor (
NewListItemExpression¶
-
SignalChartBuilder.
NewListItemExpression
¶ Creates a new list item including expression
Signature
NewListItemExpression(sensor, alwaysEvaluated, timeSensor, condition, threshold, delayTime, signal)
Parameters: - sensor (
NXOpen.Motion.MotionSensor
) – sensor - alwaysEvaluated (bool) – always evaluted
- timeSensor (int) – time sensor
- condition (int) – condition
- threshold (
NXOpen.Expression
) – threshold - delayTime (
NXOpen.Expression
) – delay time - signal (
NXOpen.Expression
) – signal
Returns: Return type: New in version NX8.5.0.
License requirements: nx_motion_motor (“NX Motion Motor”)
- sensor (
Validate¶
-
SignalChartBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.