PointOnSurfaceCollection Class¶
-
class
NXOpen.Motion.
PointOnSurfaceCollection
¶ Bases:
object
Represents a collection of Point on Surface objects
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreatePointOnSurfaceBuilder | Creates a NXOpen.Motion.PointOnSurfaceBuilder @return |
FindObject | Finds the NXOpen.Motion.PointOnSurface with the given name. |
Method Detail¶
CreatePointOnSurfaceBuilder¶
-
PointOnSurfaceCollection.
CreatePointOnSurfaceBuilder
¶ Creates a
NXOpen.Motion.PointOnSurfaceBuilder
Signature
CreatePointOnSurfaceBuilder(pointonsurface)
Parameters: pointonsurface ( NXOpen.Motion.PointOnSurface
) –Returns: Return type: NXOpen.Motion.PointOnSurfaceBuilder
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
PointOnSurfaceCollection.
FindObject
¶ Finds the
NXOpen.Motion.PointOnSurface
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.PointOnSurface
.Returns: NXOpen.Motion.PointOnSurface
with this name.Return type: NXOpen.Motion.PointOnSurface
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)