PointOnSurfaceBuilder Class¶
-
class
NXOpen.Motion.
PointOnSurfaceBuilder
¶ Bases:
NXOpen.Motion.MotionBuilder
Represents a
NXOpen.Motion.PointOnSurfaceBuilder
To create a new instance of this class, use
NXOpen.Motion.PointOnSurfaceCollection.CreatePointOnSurfaceBuilder()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
DisplayScale | Returns or sets the icon display scale |
GroupName | Returns or sets the group name |
GroupType | Returns or sets the group type |
Link | Returns the link |
Name | Returns or sets the name |
Point | Returns or sets the selected point |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFaces | Returns the selected faces @return |
GetObject | Returns the object currently being edited by this builder. |
SetFaces | Set the faces |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Link¶
-
PointOnSurfaceBuilder.
Link
¶ Returns the link
-------------------------------------
Getter Method
Signature
Link()
Returns: Return type: NXOpen.Motion.SelectLink
New in version NX8.0.0.
License requirements: None.
Name¶
-
PointOnSurfaceBuilder.
Name
¶ Returns or sets the name
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
Point¶
-
PointOnSurfaceBuilder.
Point
¶ Returns or sets the selected point
-------------------------------------
Getter Method
Signature
Point()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point(point)
Parameters: point ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
GetFaces¶
-
PointOnSurfaceBuilder.
GetFaces
¶ Returns the selected faces
Signature
GetFaces()
Returns: Return type: list of NXOpen.Face
New in version NX6.0.0.
License requirements: None.
SetFaces¶
-
PointOnSurfaceBuilder.
SetFaces
¶ Set the faces
Signature
SetFaces(faces)
Parameters: faces (list of NXOpen.Face
) –New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
Validate¶
-
PointOnSurfaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.