ConnectorBuilder Class¶
-
class
NXOpen.Motion.
ConnectorBuilder
¶ Bases:
NXOpen.Motion.MotionBuilder
Represents ConnectorBuilder
This is an abstract class, and cannot be created.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ActionLink | Returns the action link. |
ActionPoint | Returns or sets the action point. |
Attachment | Returns or sets the attachment type |
DisplayScale | Returns or sets the icon display scale |
GroupName | Returns or sets the group name |
GroupType | Returns or sets the group type |
Joint | Returns the joint . |
ReactionLink | Returns the reaction link. |
ReactionPoint | Returns or sets the reaction point. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ConnectorBuilderAttachmentType Enumeration | Definitions of connector attachment type |
Property Detail¶
ActionLink¶
-
ConnectorBuilder.
ActionLink
¶ Returns the action link.
Only valid if
Motion.ConnectorBuilderAttachmentType.Link
is set.-------------------------------------
Getter Method
Signature
ActionLink()
Returns: Return type: NXOpen.Motion.SelectLink
New in version NX6.0.0.
License requirements: None.
ActionPoint¶
-
ConnectorBuilder.
ActionPoint
¶ Returns or sets the action point.
Only valid if
Motion.ConnectorBuilderAttachmentType.Link
is set.-------------------------------------
Getter Method
Signature
ActionPoint()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActionPoint(actionPoint)
Parameters: actionPoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
Attachment¶
-
ConnectorBuilder.
Attachment
¶ Returns or sets the attachment type
-------------------------------------
Getter Method
Signature
Attachment()
Returns: Return type: NXOpen.Motion.ConnectorBuilderAttachmentType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Attachment(attachment)
Parameters: attachment ( NXOpen.Motion.ConnectorBuilderAttachmentType
) –New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
Joint¶
-
ConnectorBuilder.
Joint
¶ Returns the joint .
Only valid if
Motion.ConnectorBuilderAttachmentType.SliderJoint
orMotion.ConnectorBuilderAttachmentType.RevoluteJoint
is set.-------------------------------------
Getter Method
Signature
Joint()
Returns: Return type: NXOpen.Motion.SelectJoint
New in version NX6.0.0.
License requirements: None.
ReactionLink¶
-
ConnectorBuilder.
ReactionLink
¶ Returns the reaction link.
Only valid if
Motion.ConnectorBuilderAttachmentType.Link
is set.-------------------------------------
Getter Method
Signature
ReactionLink()
Returns: Return type: NXOpen.Motion.SelectLink
New in version NX6.0.0.
License requirements: None.
ReactionPoint¶
-
ConnectorBuilder.
ReactionPoint
¶ Returns or sets the reaction point.
Only valid if
Motion.ConnectorBuilderAttachmentType.Link
is set.-------------------------------------
Getter Method
Signature
ReactionPoint()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReactionPoint(reactionPoint)
Parameters: reactionPoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
Validate¶
-
ConnectorBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.