ConnectorBuilderAttachmentType Enumeration¶
NXOpen.Motion.ConnectorBuilder.AttachmentType is an alias for NXOpen.Motion.ConnectorBuilderAttachmentType
-
class
NXOpen.Motion.
ConnectorBuilderAttachmentType
¶ Bases:
object
Definitions of connector attachment type
Enum Members
Enum Member Enum Member Description Link connector is attacted to linksSliderJoint connector is attacted to slider jointRevoluteJoint connector is attacted to revolute joint-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-