BushingCoefficients Class¶
-
class
NXOpen.Motion.
BushingCoefficients
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a Motion BushingCoefficients
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
CylindricalCoefficients | Returns the cylindrical coefficients, it is used in Motion.BushingBuilderBushingTypes.Cylindrical case |
Tag | Returns the Tag for this object. |
TorsionalCoefficients | Returns the torsional coefficients, it is used in Motion.BushingBuilderBushingTypes.General case |
TranslationalCoefficients | Returns the translational coefficients, it is used in Motion.BushingBuilderBushingTypes.General case |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CylindricalCoefficients¶
-
BushingCoefficients.
CylindricalCoefficients
¶ Returns the cylindrical coefficients, it is used in
Motion.BushingBuilderBushingTypes.Cylindrical
case-------------------------------------
Getter Method
Signature
CylindricalCoefficients()
Returns: Return type: NXOpen.Motion.BushingCylindricalCoefficients
New in version NX6.0.0.
License requirements: None.
TorsionalCoefficients¶
-
BushingCoefficients.
TorsionalCoefficients
¶ Returns the torsional coefficients, it is used in
Motion.BushingBuilderBushingTypes.General
case-------------------------------------
Getter Method
Signature
TorsionalCoefficients()
Returns: Return type: NXOpen.Motion.BushingGeneralCoefficients
New in version NX6.0.0.
License requirements: None.
TranslationalCoefficients¶
-
BushingCoefficients.
TranslationalCoefficients
¶ Returns the translational coefficients, it is used in
Motion.BushingBuilderBushingTypes.General
case-------------------------------------
Getter Method
Signature
TranslationalCoefficients()
Returns: Return type: NXOpen.Motion.BushingGeneralCoefficients
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
BushingCoefficients.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.