BushingGeneralCoefficients Class¶
-
class
NXOpen.Motion.
BushingGeneralCoefficients
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a Motion BushingGeneralCoefficients
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
DampingCoefficients | Returns the damping coefficients, it is used in Motion.BushingBuilderBushingTypes.General case |
PreloadCoefficients | Returns the preload coefficients, it is used in Motion.BushingBuilderBushingTypes.General case. |
StiffnessCoefficients | Returns the stiffness coefficients, it is used in Motion.BushingBuilderBushingTypes.General case |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DampingCoefficients¶
-
BushingGeneralCoefficients.
DampingCoefficients
¶ Returns the damping coefficients, it is used in
Motion.BushingBuilderBushingTypes.General
case-------------------------------------
Getter Method
Signature
DampingCoefficients()
Returns: Return type: NXOpen.Motion.BushingGeneralCoefficientsComponent
New in version NX6.0.0.
License requirements: None.
PreloadCoefficients¶
-
BushingGeneralCoefficients.
PreloadCoefficients
¶ Returns the preload coefficients, it is used in
Motion.BushingBuilderBushingTypes.General
case.Preload properties only linear is supported
-------------------------------------
Getter Method
Signature
PreloadCoefficients()
Returns: Return type: NXOpen.Motion.BushingGeneralCoefficientsComponent
New in version NX6.0.0.
License requirements: None.
StiffnessCoefficients¶
-
BushingGeneralCoefficients.
StiffnessCoefficients
¶ Returns the stiffness coefficients, it is used in
Motion.BushingBuilderBushingTypes.General
case-------------------------------------
Getter Method
Signature
StiffnessCoefficients()
Returns: Return type: NXOpen.Motion.BushingGeneralCoefficientsComponent
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
BushingGeneralCoefficients.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.