SlidingJointBuilder Class¶
-
class
NXOpen.Mechatronics.
SlidingJointBuilder
¶ Bases:
NXOpen.Mechatronics.PhysicsJointBuilder
Represents a
NXOpen.Mechatronics.SlidingJoint
builder.To create a new instance of this class, use
NXOpen.Mechatronics.SlidingJointCollection.CreateSlidingJointBuilder()
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
Attachment | Returns the attachment of joint. |
Base | Returns the base of joint. |
EnableLowerLimit | Returns or sets the lower limit option. |
EnableUpperLimit | Returns or sets the upper limit option. |
FeedbackPoint | Returns or sets the position of visual feedback point. |
LowerLimit | Returns the lower limit. |
Name | Returns or sets the name. |
Offset | Returns the offset value. |
Tag | Returns the Tag for this object. |
UpperLimit | Returns the upper limit. |
Vector | Returns or sets the vector. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetAttachment | Sets the attachment. |
SetBase | Sets the base. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
EnableLowerLimit¶
-
SlidingJointBuilder.
EnableLowerLimit
¶ Returns or sets the lower limit option.
If the enable is true, then the joint will be applied a lower limit in movement.
-------------------------------------
Getter Method
Signature
EnableLowerLimit()
Returns: Return type: bool New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
EnableLowerLimit(enable)
Parameters: enable (bool) – New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
EnableUpperLimit¶
-
SlidingJointBuilder.
EnableUpperLimit
¶ Returns or sets the upper limit option.
If the enable is true, then the joint will be applied an upper limit in movement.
-------------------------------------
Getter Method
Signature
EnableUpperLimit()
Returns: Return type: bool New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
EnableUpperLimit(enable)
Parameters: enable (bool) – New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FeedbackPoint¶
-
SlidingJointBuilder.
FeedbackPoint
¶ Returns or sets the position of visual feedback point.
-------------------------------------
Getter Method
Signature
FeedbackPoint()
Returns: Return type: NXOpen.Point
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
FeedbackPoint(feedback)
Parameters: feedback ( NXOpen.Point
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
LowerLimit¶
-
SlidingJointBuilder.
LowerLimit
¶ Returns the lower limit.
The lower limit setup for joint movement.
-------------------------------------
Getter Method
Signature
LowerLimit()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Offset¶
-
SlidingJointBuilder.
Offset
¶ Returns the offset value.
-------------------------------------
Getter Method
Signature
Offset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
UpperLimit¶
-
SlidingJointBuilder.
UpperLimit
¶ Returns the upper limit.
The upper limit setup for joint movement.
-------------------------------------
Getter Method
Signature
UpperLimit()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Vector¶
-
SlidingJointBuilder.
Vector
¶ Returns or sets the vector.
-------------------------------------
Getter Method
Signature
Vector()
Returns: Return type: NXOpen.Direction
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Vector(specifyVector)
Parameters: specifyVector ( NXOpen.Direction
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Validate¶
-
SlidingJointBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.