PhysicsJointBuilder Class¶
-
class
NXOpen.Mechatronics.
PhysicsJointBuilder
¶ Bases:
NXOpen.Builder
Represents a base builder for Physics Joints.
This is an abstract class, and cannot be created.
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
Attachment | Returns the attachment of joint. |
Base | Returns the base of joint. |
Name | Returns or sets the name. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetAttachment | Sets the attachment. |
SetBase | Sets the base. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Attachment¶
-
PhysicsJointBuilder.
Attachment
¶ Returns the attachment of joint.
This can be a
NXOpen.Mechatronics.RigidBody
or objects which can create a rigid body by.-------------------------------------
Getter Method
Signature
Attachment()
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Base¶
-
PhysicsJointBuilder.
Base
¶ Returns the base of joint.
This can be a
NXOpen.Mechatronics.RigidBody
or objects which can create a rigid body by.-------------------------------------
Getter Method
Signature
Base()
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Name¶
-
PhysicsJointBuilder.
Name
¶ Returns or sets the name.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
SetAttachment¶
-
PhysicsJointBuilder.
SetAttachment
¶ Sets the attachment.
Signature
SetAttachment(attachment)
Parameters: attachment ( NXOpen.NXObject
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetBase¶
-
PhysicsJointBuilder.
SetBase
¶ Sets the base.
Signature
SetBase(base)
Parameters: base ( NXOpen.NXObject
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
PhysicsJointBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.