SelectClassificationBuilder Class¶
-
class
NXOpen.Mechatronics.
SelectClassificationBuilder
¶ Bases:
NXOpen.Tooling.SelectReuseLibraryItemBuilder
Select a classification from the reuse library.
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ClassId |
|
DescriptiveName | Returns or sets the descriptive name |
Selection | Returns or sets the path of the file from the reuse library |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
ClassId¶
-
SelectClassificationBuilder.
ClassId
¶ Returns or sets the Teamcenter storage class id.
It is the storage class ID of Teamcenter classification reuse library.
-------------------------------------
Getter Method
Signature
ClassId()
Returns: the class id Return type: str New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ClassId(classId)
Parameters: classId (str) – the class id New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)