SelectReuseLibraryItemBuilder Class¶
-
class
NXOpen.Tooling.
SelectReuseLibraryItemBuilder
¶ Bases:
NXOpen.TaggedObject
Select a part from the reuse library
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
DescriptiveName | Returns or sets the descriptive name |
Selection | Returns or sets the path of the file from the reuse library |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
DescriptiveName¶
-
SelectReuseLibraryItemBuilder.
DescriptiveName
¶ Returns or sets the descriptive name
-------------------------------------
Getter Method
Signature
DescriptiveName()
Returns: the path of a part Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DescriptiveName(descriptiveName)
Parameters: descriptiveName (str) – the path of a part New in version NX9.0.0.
License requirements: None.
Selection¶
-
SelectReuseLibraryItemBuilder.
Selection
¶ Returns or sets the path of the file from the reuse library
-------------------------------------
Getter Method
Signature
Selection()
Returns: the path of a part Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Selection(path)
Parameters: path (str) – the path of a part New in version NX9.0.0.
License requirements: None.