ReadWriteDeviceBuilder Class¶
-
class
NXOpen.Mechatronics.
ReadWriteDeviceBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.ReadWriteDeviceBuilder
.To create a new instance of this class, use
NXOpen.Mechatronics.ReadWriteDeviceCollection.CreateReadWriteDeviceBuilder()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Name | Returns or sets the name. |
Sensor | Returns the selected sensor NXOpen.Mechatronics.CollisionSensor object. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDeviceType | Gets device type. |
GetExecuteMode | Gets execute mode. |
GetForm | Gets the form NXOpen.Mechatronics.TagFormObject object. |
GetObject | Returns the object currently being edited by this builder. |
GetTable | Gets the table NXOpen.Mechatronics.TagTableObject object. |
SetDeviceType | Sets device type. |
SetExecuteMode | Sets execute mode. |
SetForm | Sets the form NXOpen.Mechatronics.TagFormObject object. |
SetTable | Sets the table NXOpen.Mechatronics.TagTableObject object. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ReadWriteDeviceBuilderDeviceType Enumeration | the device types. |
ReadWriteDeviceBuilderExecuteMode Enumeration | the execute modes. |
Property Detail¶
Name¶
-
ReadWriteDeviceBuilder.
Name
¶ Returns or sets the name.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Sensor¶
-
ReadWriteDeviceBuilder.
Sensor
¶ Returns the selected sensor
NXOpen.Mechatronics.CollisionSensor
object.-------------------------------------
Getter Method
Signature
Sensor()
Returns: Return type: NXOpen.Mechatronics.SelectCollisionSensor
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
GetDeviceType¶
-
ReadWriteDeviceBuilder.
GetDeviceType
¶ Gets device type.
Signature
GetDeviceType()
Returns: Return type: NXOpen.Mechatronics.ReadWriteDeviceBuilderDeviceType
New in version NX10.0.0.
License requirements: None.
GetExecuteMode¶
-
ReadWriteDeviceBuilder.
GetExecuteMode
¶ Gets execute mode.
Signature
GetExecuteMode()
Returns: Return type: NXOpen.Mechatronics.ReadWriteDeviceBuilderExecuteMode
New in version NX10.0.0.
License requirements: None.
GetForm¶
-
ReadWriteDeviceBuilder.
GetForm
¶ Gets the form
NXOpen.Mechatronics.TagFormObject
object.Signature
GetForm()
Returns: Return type: NXOpen.Mechatronics.TagFormObject
New in version NX10.0.0.
License requirements: None.
GetTable¶
-
ReadWriteDeviceBuilder.
GetTable
¶ Gets the table
NXOpen.Mechatronics.TagTableObject
object.Signature
GetTable()
Returns: Return type: NXOpen.Mechatronics.TagTableObject
New in version NX10.0.0.
License requirements: None.
SetDeviceType¶
-
ReadWriteDeviceBuilder.
SetDeviceType
¶ Sets device type.
Signature
SetDeviceType(type)
Parameters: type ( NXOpen.Mechatronics.ReadWriteDeviceBuilderDeviceType
) –New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetExecuteMode¶
-
ReadWriteDeviceBuilder.
SetExecuteMode
¶ Sets execute mode.
Signature
SetExecuteMode(mode)
Parameters: mode ( NXOpen.Mechatronics.ReadWriteDeviceBuilderExecuteMode
) –New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetForm¶
-
ReadWriteDeviceBuilder.
SetForm
¶ Sets the form
NXOpen.Mechatronics.TagFormObject
object.Signature
SetForm(form)
Parameters: form ( NXOpen.Mechatronics.TagFormObject
) –New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetTable¶
-
ReadWriteDeviceBuilder.
SetTable
¶ Sets the table
NXOpen.Mechatronics.TagTableObject
object.Signature
SetTable(table)
Parameters: table ( NXOpen.Mechatronics.TagTableObject
) –New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
ReadWriteDeviceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.