ReadWriteDeviceBuilderDeviceType Enumeration

NXOpen.Mechatronics.ReadWriteDeviceBuilder.DeviceType is an alias for NXOpen.Mechatronics.ReadWriteDeviceBuilderDeviceType

class NXOpen.Mechatronics.ReadWriteDeviceBuilderDeviceType

Bases: object

the device types.

Enum Members

Enum Member Enum Member Description
Reader
Reader
Writer
Writer
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.