PreferencesBuilder Class¶
-
class
NXOpen.Mechatronics.
PreferencesBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.PreferencesBuilder
builder.To create a new instance of this class, use
NXOpen.Mechatronics.PhysicsPreferenceCollection.CreatePreferenceBuilder()
Default values.
Property Value AngularDampingExpression.Value 3490.6585 (millimeters part), 0.030895 (inches part) CoSimulation false CollisionPrecisionExpression.Value 0.1 (millimeters part), 0.0039 (inches part) ConnectURL DynamicFrictionExpression.Value 0.7 EnableTimeSync false ErrorReductionExpression.Value 50 Gx.Value 0 (millimeters part), 0 (inches part) Gy.Value 0 (millimeters part), 0 (inches part) Gz.Value -9806.65 (millimeters part), -386.09 (inches part) LinearDampingExpression.Value 0.05 (millimeters part), 0.0002855 (inches part) MaxIterationExpression.Value 100 RestitutionExpression.Value 0.01 RollingFrictionExpression.Value 0.0 SpringForceMultiplierExpression.Value 100 StaticFrictionExpression.Value 0.7 StepTimeExpression.Value 0.001 ToleranceExpression.Value 0.1 (millimeters part), 0.0039 (inches part) New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
AngularDampingExpression | Returns the angular damping expression |
CoSimulation | Returns or sets the co-simulation option |
CollisionPrecision | Returns or sets the collision precision. |
CollisionPrecisionExpression | Returns the Collision Precision Expression |
ConnectURL | Returns or sets the Simit Connect URL string |
DynamicFriction | Returns or sets the dynamic friction. |
DynamicFrictionExpression | Returns the Dynamic Friction Expression |
EnableTimeSync | Returns or sets the time synchronization option |
ErrorReduction | Returns or sets the error reduction. |
ErrorReductionExpression | Returns the Error Reduction Expression |
FilePicker | Returns or sets the export timing chart file path |
ForwardStepTime | Returns the Forward Step Time Expression |
GeometryHighlight | Returns or sets the geometry highlight on collsion. |
Gx | Returns the gx. |
Gy | Returns the gy. |
Gz | Returns the gz. |
InvokeExport | Returns or sets the toggle value for the invoke timing chart after import |
LinearDampingExpression | Returns the linear damping expression |
LoadAsSaved | Returns or sets the load as saved option for MCD Objects. |
MasterType | Returns or sets the master type option |
MaxIteration | Returns or sets the max iteration. |
MaxIterationExpression | Returns the Maximum Iteration Expression |
RefreshPrecision | Returns or sets the inspector refresh precision. |
Restitution | Returns or sets the restitution. |
RestitutionExpression | Returns the Restitution Expression |
RevisionRule | Returns or sets the revision rule for MCD Objects. |
RollingFrictionExpression | Returns the rolling Friction Expression |
ShapeHighlight | Returns or sets the shape highlight on collsion. |
SpringForceMultiplier | Returns or sets the spring force multiplier. |
SpringForceMultiplierExpression | Returns the Spring Force Multiplier Expression |
StaticFriction | Returns or sets the static friction. |
StaticFrictionExpression | Returns the static Friction Expression |
StepTime | Returns or sets the step time. |
StepTimeExpression | Returns the Step Time Expression |
StickyFactor | Returns or sets the sticky factor. |
StickyForce | Returns the sticky factor Expression |
SynchronizationTime | Returns the time interval to do synchronization with SIMIT |
Tag | Returns the Tag for this object. |
TimeScaleFactor | Returns or sets the time scale factor |
Tolerance | Returns or sets the tolerance. |
ToleranceExpression | Returns the Tolerance Expression |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PreferencesBuilderMasterTypes Enumeration | the Co-Simulation master type. |
Property Detail¶
AngularDampingExpression¶
-
PreferencesBuilder.
AngularDampingExpression
¶ Returns the angular damping expression
-------------------------------------
Getter Method
Signature
AngularDampingExpression()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
CoSimulation¶
-
PreferencesBuilder.
CoSimulation
¶ Returns or sets the co-simulation option
-------------------------------------
Getter Method
Signature
CoSimulation()
Returns: Return type: bool New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
CoSimulation(coSimulation)
Parameters: coSimulation (bool) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
CollisionPrecision¶
-
PreferencesBuilder.
CollisionPrecision
¶ Returns or sets the collision precision.
-------------------------------------
Getter Method
Signature
CollisionPrecision()
Returns: Return type: float New in version NX7.5.1.
Deprecated since version NX9.0.0: Use
NXOpen.Mechatronics.PreferencesBuilder.CollisionPrecisionExpression()
insteadLicense requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
CollisionPrecision(collisionPrecision)
Parameters: collisionPrecision (float) – New in version NX7.5.1.
Deprecated since version NX9.0.0: This functionality is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
CollisionPrecisionExpression¶
-
PreferencesBuilder.
CollisionPrecisionExpression
¶ Returns the Collision Precision Expression
-------------------------------------
Getter Method
Signature
CollisionPrecisionExpression()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ConnectURL¶
-
PreferencesBuilder.
ConnectURL
¶ Returns or sets the Simit Connect URL string
-------------------------------------
Getter Method
Signature
ConnectURL()
Returns: Return type: str New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ConnectURL(connectURL)
Parameters: connectURL (str) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
DynamicFriction¶
-
PreferencesBuilder.
DynamicFriction
¶ Returns or sets the dynamic friction.
-------------------------------------
Getter Method
Signature
DynamicFriction()
Returns: Return type: float New in version NX7.5.1.
Deprecated since version NX9.0.0: Use
NXOpen.Mechatronics.PreferencesBuilder.DynamicFrictionExpression()
insteadLicense requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
DynamicFriction(dynamicFriction)
Parameters: dynamicFriction (float) – New in version NX7.5.1.
Deprecated since version NX9.0.0: This functionality is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
DynamicFrictionExpression¶
-
PreferencesBuilder.
DynamicFrictionExpression
¶ Returns the Dynamic Friction Expression
-------------------------------------
Getter Method
Signature
DynamicFrictionExpression()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
EnableTimeSync¶
-
PreferencesBuilder.
EnableTimeSync
¶ Returns or sets the time synchronization option
-------------------------------------
Getter Method
Signature
EnableTimeSync()
Returns: Return type: bool New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
EnableTimeSync(enableTimeSync)
Parameters: enableTimeSync (bool) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ErrorReduction¶
-
PreferencesBuilder.
ErrorReduction
¶ Returns or sets the error reduction.
-------------------------------------
Getter Method
Signature
ErrorReduction()
Returns: Return type: float New in version NX7.5.1.
Deprecated since version NX9.0.0: Use
NXOpen.Mechatronics.PreferencesBuilder.ErrorReductionExpression()
insteadLicense requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ErrorReduction(errorReduction)
Parameters: errorReduction (float) – New in version NX7.5.1.
Deprecated since version NX9.0.0: This functionality is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ErrorReductionExpression¶
-
PreferencesBuilder.
ErrorReductionExpression
¶ Returns the Error Reduction Expression
-------------------------------------
Getter Method
Signature
ErrorReductionExpression()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FilePicker¶
-
PreferencesBuilder.
FilePicker
¶ Returns or sets the export timing chart file path
-------------------------------------
Getter Method
Signature
FilePicker()
Returns: Return type: str New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
FilePicker(exportFile)
Parameters: exportFile (str) – New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ForwardStepTime¶
-
PreferencesBuilder.
ForwardStepTime
¶ Returns the Forward Step Time Expression
-------------------------------------
Getter Method
Signature
ForwardStepTime()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
GeometryHighlight¶
-
PreferencesBuilder.
GeometryHighlight
¶ Returns or sets the geometry highlight on collsion.
-------------------------------------
Getter Method
Signature
GeometryHighlight()
Returns: Return type: bool New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
GeometryHighlight(highlight)
Parameters: highlight (bool) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Gx¶
-
PreferencesBuilder.
Gx
¶ Returns the gx.
-------------------------------------
Getter Method
Signature
Gx()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Gy¶
-
PreferencesBuilder.
Gy
¶ Returns the gy.
-------------------------------------
Getter Method
Signature
Gy()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Gz¶
-
PreferencesBuilder.
Gz
¶ Returns the gz.
-------------------------------------
Getter Method
Signature
Gz()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
InvokeExport¶
-
PreferencesBuilder.
InvokeExport
¶ Returns or sets the toggle value for the invoke timing chart after import
-------------------------------------
Getter Method
Signature
InvokeExport()
Returns: Return type: bool New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
InvokeExport(param)
Parameters: param (bool) – New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
LinearDampingExpression¶
-
PreferencesBuilder.
LinearDampingExpression
¶ Returns the linear damping expression
-------------------------------------
Getter Method
Signature
LinearDampingExpression()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
LoadAsSaved¶
-
PreferencesBuilder.
LoadAsSaved
¶ Returns or sets the load as saved option for MCD Objects.
-------------------------------------
Getter Method
Signature
LoadAsSaved()
Returns: Return type: bool New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
LoadAsSaved(loadAsSaved)
Parameters: loadAsSaved (bool) – New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
MasterType¶
-
PreferencesBuilder.
MasterType
¶ Returns or sets the master type option
-------------------------------------
Getter Method
Signature
MasterType()
Returns: Return type: NXOpen.Mechatronics.PreferencesBuilderMasterTypes
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
MasterType(masterType)
Parameters: masterType ( NXOpen.Mechatronics.PreferencesBuilderMasterTypes
) –New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
MaxIteration¶
-
PreferencesBuilder.
MaxIteration
¶ Returns or sets the max iteration.
-------------------------------------
Getter Method
Signature
MaxIteration()
Returns: Return type: int New in version NX7.5.1.
Deprecated since version NX9.0.0: Use
NXOpen.Mechatronics.PreferencesBuilder.MaxIterationExpression()
insteadLicense requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
MaxIteration(maxIter)
Parameters: maxIter (int) – New in version NX7.5.1.
Deprecated since version NX9.0.0: This functionality is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
MaxIterationExpression¶
-
PreferencesBuilder.
MaxIterationExpression
¶ Returns the Maximum Iteration Expression
-------------------------------------
Getter Method
Signature
MaxIterationExpression()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RefreshPrecision¶
-
PreferencesBuilder.
RefreshPrecision
¶ Returns or sets the inspector refresh precision.
This option specifies the refresh precision to be used by the inspector to determine whether to update property values in UI or not.
-------------------------------------
Getter Method
Signature
RefreshPrecision()
Returns: Return type: float New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
RefreshPrecision(refreshPrecision)
Parameters: refreshPrecision (float) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Restitution¶
-
PreferencesBuilder.
Restitution
¶ Returns or sets the restitution.
-------------------------------------
Getter Method
Signature
Restitution()
Returns: Return type: float New in version NX7.5.1.
Deprecated since version NX9.0.0: Use
NXOpen.Mechatronics.PreferencesBuilder.RestitutionExpression()
insteadLicense requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Restitution(restitution)
Parameters: restitution (float) – New in version NX7.5.1.
Deprecated since version NX9.0.0: This functionality is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RestitutionExpression¶
-
PreferencesBuilder.
RestitutionExpression
¶ Returns the Restitution Expression
-------------------------------------
Getter Method
Signature
RestitutionExpression()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RevisionRule¶
-
PreferencesBuilder.
RevisionRule
¶ Returns or sets the revision rule for MCD Objects.
-------------------------------------
Getter Method
Signature
RevisionRule()
Returns: Return type: str New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
RevisionRule(revisionRule)
Parameters: revisionRule (str) – New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RollingFrictionExpression¶
-
PreferencesBuilder.
RollingFrictionExpression
¶ Returns the rolling Friction Expression
-------------------------------------
Getter Method
Signature
RollingFrictionExpression()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ShapeHighlight¶
-
PreferencesBuilder.
ShapeHighlight
¶ Returns or sets the shape highlight on collsion.
-------------------------------------
Getter Method
Signature
ShapeHighlight()
Returns: Return type: bool New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ShapeHighlight(highlight)
Parameters: highlight (bool) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SpringForceMultiplier¶
-
PreferencesBuilder.
SpringForceMultiplier
¶ Returns or sets the spring force multiplier.
-------------------------------------
Getter Method
Signature
SpringForceMultiplier()
Returns: Return type: float New in version NX7.5.1.
Deprecated since version NX9.0.0: Use
NXOpen.Mechatronics.PreferencesBuilder.SpringForceMultiplierExpression()
insteadLicense requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
SpringForceMultiplier(springForceMultiplier)
Parameters: springForceMultiplier (float) – New in version NX7.5.1.
Deprecated since version NX9.0.0: This functionality is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SpringForceMultiplierExpression¶
-
PreferencesBuilder.
SpringForceMultiplierExpression
¶ Returns the Spring Force Multiplier Expression
-------------------------------------
Getter Method
Signature
SpringForceMultiplierExpression()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
StaticFriction¶
-
PreferencesBuilder.
StaticFriction
¶ Returns or sets the static friction.
-------------------------------------
Getter Method
Signature
StaticFriction()
Returns: Return type: float New in version NX7.5.1.
Deprecated since version NX9.0.0: Use
NXOpen.Mechatronics.PreferencesBuilder.StaticFrictionExpression()
insteadLicense requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
StaticFriction(staticFriction)
Parameters: staticFriction (float) – New in version NX7.5.1.
Deprecated since version NX9.0.0: This functionality is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
StaticFrictionExpression¶
-
PreferencesBuilder.
StaticFrictionExpression
¶ Returns the static Friction Expression
-------------------------------------
Getter Method
Signature
StaticFrictionExpression()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
StepTime¶
-
PreferencesBuilder.
StepTime
¶ Returns or sets the step time.
-------------------------------------
Getter Method
Signature
StepTime()
Returns: Return type: float New in version NX7.5.1.
Deprecated since version NX9.0.0: Use
NXOpen.Mechatronics.PreferencesBuilder.StepTimeExpression()
insteadLicense requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
StepTime(stepTime)
Parameters: stepTime (float) – New in version NX7.5.1.
Deprecated since version NX9.0.0: This functionality is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
StepTimeExpression¶
-
PreferencesBuilder.
StepTimeExpression
¶ Returns the Step Time Expression
-------------------------------------
Getter Method
Signature
StepTimeExpression()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
StickyFactor¶
-
PreferencesBuilder.
StickyFactor
¶ Returns or sets the sticky factor.
-------------------------------------
Getter Method
Signature
StickyFactor()
Returns: Return type: float New in version NX10.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Mechatronics.PreferencesBuilder.StickyForce()
instead.License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
StickyFactor(factor)
Parameters: factor (float) – New in version NX10.0.0.
Deprecated since version NX11.0.0: This functionality is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
StickyForce¶
-
PreferencesBuilder.
StickyForce
¶ Returns the sticky factor Expression
-------------------------------------
Getter Method
Signature
StickyForce()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SynchronizationTime¶
-
PreferencesBuilder.
SynchronizationTime
¶ Returns the time interval to do synchronization with SIMIT
-------------------------------------
Getter Method
Signature
SynchronizationTime()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
TimeScaleFactor¶
-
PreferencesBuilder.
TimeScaleFactor
¶ Returns or sets the time scale factor
-------------------------------------
Getter Method
Signature
TimeScaleFactor()
Returns: Return type: float New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
TimeScaleFactor(scaleFactor)
Parameters: scaleFactor (float) – New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Tolerance¶
-
PreferencesBuilder.
Tolerance
¶ Returns or sets the tolerance.
-------------------------------------
Getter Method
Signature
Tolerance()
Returns: Return type: float New in version NX7.5.1.
Deprecated since version NX9.0.0: Use
NXOpen.Mechatronics.PreferencesBuilder.ToleranceExpression()
insteadLicense requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Tolerance(tolerance)
Parameters: tolerance (float) – New in version NX7.5.1.
Deprecated since version NX9.0.0: This functionality is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ToleranceExpression¶
-
PreferencesBuilder.
ToleranceExpression
¶ Returns the Tolerance Expression
-------------------------------------
Getter Method
Signature
ToleranceExpression()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Validate¶
-
PreferencesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.