PreferencesBuilderMasterTypes Enumeration

NXOpen.Mechatronics.PreferencesBuilder.MasterTypes is an alias for NXOpen.Mechatronics.PreferencesBuilderMasterTypes

class NXOpen.Mechatronics.PreferencesBuilderMasterTypes

Bases: object

the Co-Simulation master type.

Enum Members

Enum Member Enum Member Description
Mcd
MCD
Simit
SIMIT
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.