LinearSpringJointBuilder Class¶
-
class
NXOpen.Mechatronics.
LinearSpringJointBuilder
¶ Bases:
NXOpen.Mechatronics.PhysicsJointBuilder
Represents a
NXOpen.Mechatronics.LinearSpringJoint
builder.To create a new instance of this class, use
NXOpen.Mechatronics.LinearSpringJointCollection.CreateLinearSpringJointBuilder()
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
Attachment | Returns the attachment of joint. |
AttachmentPoint | Returns or sets the attachment point. |
Base | Returns the base of joint. |
BasePoint | Returns or sets the base point. |
Damping | Returns the damping. |
Name | Returns or sets the name. |
RelaxedPosition | Returns the relaxed position. |
SpringConstant | Returns the spring constant. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetAttachment | Sets the attachment. |
SetBase | Sets the base. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AttachmentPoint¶
-
LinearSpringJointBuilder.
AttachmentPoint
¶ Returns or sets the attachment point.
-------------------------------------
Getter Method
Signature
AttachmentPoint()
Returns: Return type: NXOpen.Point
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
AttachmentPoint(attachmentPoint)
Parameters: attachmentPoint ( NXOpen.Point
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
BasePoint¶
-
LinearSpringJointBuilder.
BasePoint
¶ Returns or sets the base point.
-------------------------------------
Getter Method
Signature
BasePoint()
Returns: Return type: NXOpen.Point
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
BasePoint(basePoint)
Parameters: basePoint ( NXOpen.Point
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Damping¶
-
LinearSpringJointBuilder.
Damping
¶ Returns the damping.
-------------------------------------
Getter Method
Signature
Damping()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RelaxedPosition¶
-
LinearSpringJointBuilder.
RelaxedPosition
¶ Returns the relaxed position.
-------------------------------------
Getter Method
Signature
RelaxedPosition()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SpringConstant¶
-
LinearSpringJointBuilder.
SpringConstant
¶ Returns the spring constant.
-------------------------------------
Getter Method
Signature
SpringConstant()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Validate¶
-
LinearSpringJointBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.