InclinometerCollection Class¶
-
class
NXOpen.Mechatronics.
InclinometerCollection
¶ Bases:
object
Represents a collection of Inclinometer.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateInclinometerBuilder |
|
FindObject |
|
Method Detail¶
CreateInclinometerBuilder¶
-
InclinometerCollection.
CreateInclinometerBuilder
¶ Creates a
NXOpen.Mechatronics.InclinometerBuilder
.Signature
CreateInclinometerBuilder(inclinometer)
Parameters: inclinometer ( NXOpen.Mechatronics.Inclinometer
) –NXOpen.Mechatronics.Inclinometer
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.InclinometerBuilder
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
InclinometerCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.Inclinometer
with the given name. An exception will be thrown if no object can be found with given name.Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.Inclinometer
.Returns: NXOpen.Mechatronics.Inclinometer
with this name.Return type: NXOpen.Mechatronics.Inclinometer
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)