InclinometerBuilder Class¶
-
class
NXOpen.Mechatronics.
InclinometerBuilder
¶ Bases:
NXOpen.Mechatronics.PhysicsConstraintBuilder
Represents a
NXOpen.Mechatronics.Inclinometer
builder.To create a new instance of this class, use
NXOpen.Mechatronics.InclinometerCollection.CreateInclinometerBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
AngleType |
|
LowerOutputRange |
|
LowerTrimRange |
|
MeasureType |
|
Name | Returns or sets the name. |
Orientation |
|
RigidBody |
|
Tag | Returns the Tag for this object. |
UpperOutputRange |
|
UpperTrimRange |
|
UseScale |
|
UseTrim |
|
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
InclinometerBuilderOutputAngleType Enumeration |
|
InclinometerBuilderOutputMeasureType Enumeration |
|
Property Detail¶
AngleType¶
-
InclinometerBuilder.
AngleType
¶ Returns or sets the angle type.
-------------------------------------
Getter Method
Signature
AngleType()
Returns: Return type: NXOpen.Mechatronics.InclinometerBuilderOutputAngleType
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
AngleType(angleType)
Parameters: angleType ( NXOpen.Mechatronics.InclinometerBuilderOutputAngleType
) –New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
LowerOutputRange¶
-
InclinometerBuilder.
LowerOutputRange
¶ Returns the lower output range used to scale the Inclinometer data. Its measure type contains constant, voltage, current
-------------------------------------
Getter Method
Signature
LowerOutputRange()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
LowerTrimRange¶
-
InclinometerBuilder.
LowerTrimRange
¶ Returns the lower trim range used to trim the Inclinometer data.
-------------------------------------
Getter Method
Signature
LowerTrimRange()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
MeasureType¶
-
InclinometerBuilder.
MeasureType
¶ Returns or sets the measure type.
-------------------------------------
Getter Method
Signature
MeasureType()
Returns: Return type: NXOpen.Mechatronics.InclinometerBuilderOutputMeasureType
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
MeasureType(measureType)
Parameters: measureType ( NXOpen.Mechatronics.InclinometerBuilderOutputMeasureType
) –New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Orientation¶
-
InclinometerBuilder.
Orientation
¶ Returns or sets the orientation.
-------------------------------------
Getter Method
Signature
Orientation()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Orientation(orientation)
Parameters: orientation ( NXOpen.CoordinateSystem
) –New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RigidBody¶
-
InclinometerBuilder.
RigidBody
¶ Returns the Rigid Body. This can be a
NXOpen.Mechatronics.RigidBody
.-------------------------------------
Getter Method
Signature
RigidBody()
Returns: Return type: NXOpen.Mechatronics.SelectRigidBody
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
UpperOutputRange¶
-
InclinometerBuilder.
UpperOutputRange
¶ Returns the upper output range used to scale the Inclinometer data.
-------------------------------------
Getter Method
Signature
UpperOutputRange()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
UpperTrimRange¶
-
InclinometerBuilder.
UpperTrimRange
¶ Returns the upper trim range used to trim the Inclinometer data.
-------------------------------------
Getter Method
Signature
UpperTrimRange()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
UseScale¶
-
InclinometerBuilder.
UseScale
¶ Returns or sets the use scale flag, which is used to control if the inclinometer includes scale parameters.
-------------------------------------
Getter Method
Signature
UseScale()
Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
UseScale(useScale)
Parameters: useScale (bool) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
UseTrim¶
-
InclinometerBuilder.
UseTrim
¶ Returns or sets the use trim flag, which is used to control if the inclinometer includes trim parameters.
-------------------------------------
Getter Method
Signature
UseTrim()
Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
UseTrim(useTrim)
Parameters: useTrim (bool) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Validate¶
-
InclinometerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.