GearBuilder Class¶
-
class
NXOpen.Mechatronics.
GearBuilder
¶ Bases:
NXOpen.Mechatronics.CouplingBuilder
Represents a
NXOpen.Mechatronics.Gear
builder.To create a new instance of this class, use
NXOpen.Mechatronics.GearCollection.CreateGearBuilder()
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
AllowSlip | Returns or sets the coulping can slip or not. |
AxisType | Returns or sets the axis joint type. |
ExpressionMasterMultiple | Returns the master multiple expression. |
ExpressionSlaveMultiple | Returns the slave multiple expression. |
MasterAxisJoint | Returns the master axis joint. |
MasterMultiple | Returns or sets the master multiple. |
Name | Returns or sets the name. |
SlaveAxisJoint | Returns the slave axis joint. |
SlaveMultiple | Returns or sets the slave multiple. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetMasterAxisJoint | Sets the master axis. |
SetSlaveAxisJoint | Sets the slave axis. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
GearBuilderAxisJointType Enumeration | the axis joint types. |
Property Detail¶
AxisType¶
-
GearBuilder.
AxisType
¶ Returns or sets the axis joint type.
-------------------------------------
Getter Method
Signature
AxisType()
Returns: Return type: NXOpen.Mechatronics.GearBuilderAxisJointType
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
AxisType(axisType)
Parameters: axisType ( NXOpen.Mechatronics.GearBuilderAxisJointType
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ExpressionMasterMultiple¶
-
GearBuilder.
ExpressionMasterMultiple
¶ Returns the master multiple expression.
-------------------------------------
Getter Method
Signature
ExpressionMasterMultiple()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ExpressionSlaveMultiple¶
-
GearBuilder.
ExpressionSlaveMultiple
¶ Returns the slave multiple expression.
-------------------------------------
Getter Method
Signature
ExpressionSlaveMultiple()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
MasterMultiple¶
-
GearBuilder.
MasterMultiple
¶ Returns or sets the master multiple.
-------------------------------------
Getter Method
Signature
MasterMultiple()
Returns: Return type: float New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
MasterMultiple(masterMultiple)
Parameters: masterMultiple (float) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SlaveMultiple¶
-
GearBuilder.
SlaveMultiple
¶ Returns or sets the slave multiple.
-------------------------------------
Getter Method
Signature
SlaveMultiple()
Returns: Return type: float New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
SlaveMultiple(slaveMultiple)
Parameters: slaveMultiple (float) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Validate¶
-
GearBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.