CouplingBuilder Class¶
-
class
NXOpen.Mechatronics.
CouplingBuilder
¶ Bases:
NXOpen.Mechatronics.PhysicsConstraintBuilder
This is an abstract class, and cannot be created.
This is an abstract class, and cannot be created.
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
AllowSlip | Returns or sets the coulping can slip or not. |
MasterAxisJoint | Returns the master axis joint. |
Name | Returns or sets the name. |
SlaveAxisJoint | Returns the slave axis joint. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetMasterAxisJoint | Sets the master axis. |
SetSlaveAxisJoint | Sets the slave axis. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AllowSlip¶
-
CouplingBuilder.
AllowSlip
¶ Returns or sets the coulping can slip or not.
-------------------------------------
Getter Method
Signature
AllowSlip()
Returns: Return type: bool New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
AllowSlip(allowSlip)
Parameters: allowSlip (bool) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
MasterAxisJoint¶
-
CouplingBuilder.
MasterAxisJoint
¶ Returns the master axis joint.
This can be a
NXOpen.Mechatronics.HingeJoint
,NXOpen.Mechatronics.SlidingJoint
andNXOpen.Mechatronics.CylindricalJoint
.-------------------------------------
Getter Method
Signature
MasterAxisJoint()
Returns: Return type: NXOpen.Mechatronics.SelectPhysicsJoint
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SlaveAxisJoint¶
-
CouplingBuilder.
SlaveAxisJoint
¶ Returns the slave axis joint.
This can be a
NXOpen.Mechatronics.HingeJoint
,NXOpen.Mechatronics.SlidingJoint
andNXOpen.Mechatronics.CylindricalJoint
.-------------------------------------
Getter Method
Signature
SlaveAxisJoint()
Returns: Return type: NXOpen.Mechatronics.SelectPhysicsJoint
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
SetMasterAxisJoint¶
-
CouplingBuilder.
SetMasterAxisJoint
¶ Sets the master axis.
Signature
SetMasterAxisJoint(master)
Parameters: master ( NXOpen.Mechatronics.PhysicsJoint
) –New in version NX8.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetSlaveAxisJoint¶
-
CouplingBuilder.
SetSlaveAxisJoint
¶ Sets the slave axis.
Signature
SetSlaveAxisJoint(slave)
Parameters: slave ( NXOpen.Mechatronics.PhysicsJoint
) –New in version NX8.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
CouplingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.