ExpressionBlockBuilder Class¶
-
class
NXOpen.Mechatronics.
ExpressionBlockBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.ExpressionBlockBuilder
builder.ExpressionBlockBuilder is used to maintain the
NXOpen.Mechatronics.ExpressionBlockObject
which is used store related expressions that work for same task.To create a new instance of this class, use
NXOpen.Mechatronics.ExpressionBlockCollection.CreateExpressionBlockBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
Name |
|
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDescription |
|
GetObject | Returns the object currently being edited by this builder. |
GetSlots |
|
LoadFromXmlFile |
|
SaveToXmlFile |
|
SetDescription |
|
SetSlots |
|
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ExpressionBlockBuilderDataType Enumeration |
|
ExpressionBlockBuilderSlotType Enumeration |
|
Structs¶
ExpressionBlockBuilderSlot_Struct Struct |
|
Property Detail¶
Name¶
-
ExpressionBlockBuilder.
Name
¶ Returns or sets the name.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
GetDescription¶
-
ExpressionBlockBuilder.
GetDescription
¶ Gets description lines.
Signature
GetDescription()
Returns: Return type: list of str New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
GetSlots¶
-
ExpressionBlockBuilder.
GetSlots
¶ Gets all Slots.
Signature
GetSlots()
Returns: Array of Slots Return type: list of NXOpen.Mechatronics.ExpressionBlockBuilderSlot_Struct
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
LoadFromXmlFile¶
-
ExpressionBlockBuilder.
LoadFromXmlFile
¶ Load data from xml file.
Signature
LoadFromXmlFile(templateFile)
Parameters: templateFile (str) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SaveToXmlFile¶
-
ExpressionBlockBuilder.
SaveToXmlFile
¶ Save data to xml file.
Signature
SaveToXmlFile(templateFile)
Parameters: templateFile (str) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetDescription¶
-
ExpressionBlockBuilder.
SetDescription
¶ Sets description lines.
Signature
SetDescription(descLines)
Parameters: descLines (list of str) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetSlots¶
-
ExpressionBlockBuilder.
SetSlots
¶ Sets all Slots.
Signature
SetSlots(slots)
Parameters: slots (list of NXOpen.Mechatronics.ExpressionBlockBuilderSlot_Struct
) – Array of SlotsNew in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
ExpressionBlockBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.