ExpressionBlockBuilderSlotType Enumeration¶
NXOpen.Mechatronics.ExpressionBlockBuilder.SlotType is an alias for NXOpen.Mechatronics.ExpressionBlockBuilderSlotType
-
class
NXOpen.Mechatronics.
ExpressionBlockBuilderSlotType
¶ Bases:
object
Represents the Slot type.
Enum Members
Enum Member Enum Member Description NotSet NoneInput Input that should connect to runtime parameter as input value.Output Output that should connect to runtime parameter to output valueParam Param that is used to configure the block to differentiate modeState State that is change during runtime based on internal dataCustom Custom that represents the user created temporary variableNum Total Num-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-