CylindricalJointBuilder Class¶
-
class
NXOpen.Mechatronics.
CylindricalJointBuilder
¶ Bases:
NXOpen.Mechatronics.PhysicsJointBuilder
Represents a
NXOpen.Mechatronics.CylindricalJoint
builder.To create a new instance of this class, use
NXOpen.Mechatronics.CylindricalJointCollection.CreateCylindricalJointBuilder()
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
AnchorPoint | Returns or sets the anchor point. |
AngularLowerLimit | Returns the angular lower limit. |
AngularUpperLimit | Returns the angular upper limit. |
Attachment | Returns the attachment of joint. |
AxisVector | Returns or sets the axis vector. |
Base | Returns the base of joint. |
EnableAngularLowerLimit | Returns or sets the angular lower limit option. |
EnableAngularUpperLimit | Returns or sets the angular upper limit option. |
EnableLinearLowerLimit | Returns or sets the linear lower limit option. |
EnableLinearUpperLimit | Returns or sets the linear upper limit option. |
LinearLowerLimit | Returns the linear lower limit. |
LinearUpperLimit | Returns the linear upper limit. |
Name | Returns or sets the name. |
Offset | Returns the offset value. |
StartAngle | Returns the start angle. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetAttachment | Sets the attachment. |
SetBase | Sets the base. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AnchorPoint¶
-
CylindricalJointBuilder.
AnchorPoint
¶ Returns or sets the anchor point.
-------------------------------------
Getter Method
Signature
AnchorPoint()
Returns: Return type: NXOpen.Point
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
AnchorPoint(anchorPoint)
Parameters: anchorPoint ( NXOpen.Point
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
AngularLowerLimit¶
-
CylindricalJointBuilder.
AngularLowerLimit
¶ Returns the angular lower limit.
The lower limit setup for joint angular movement.
-------------------------------------
Getter Method
Signature
AngularLowerLimit()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
AngularUpperLimit¶
-
CylindricalJointBuilder.
AngularUpperLimit
¶ Returns the angular upper limit.
The upper limit setup for joint angular movement.
-------------------------------------
Getter Method
Signature
AngularUpperLimit()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
AxisVector¶
-
CylindricalJointBuilder.
AxisVector
¶ Returns or sets the axis vector.
-------------------------------------
Getter Method
Signature
AxisVector()
Returns: Return type: NXOpen.Direction
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
AxisVector(axisVector)
Parameters: axisVector ( NXOpen.Direction
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
EnableAngularLowerLimit¶
-
CylindricalJointBuilder.
EnableAngularLowerLimit
¶ Returns or sets the angular lower limit option.
If the enable is true, then this joint will be applied the lower limit in angular direction.
-------------------------------------
Getter Method
Signature
EnableAngularLowerLimit()
Returns: Return type: bool New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
EnableAngularLowerLimit(enable)
Parameters: enable (bool) – New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
EnableAngularUpperLimit¶
-
CylindricalJointBuilder.
EnableAngularUpperLimit
¶ Returns or sets the angular upper limit option.
If the enable is true, then this joint will be applied the upper limit in angular direction.
-------------------------------------
Getter Method
Signature
EnableAngularUpperLimit()
Returns: Return type: bool New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
EnableAngularUpperLimit(enable)
Parameters: enable (bool) – New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
EnableLinearLowerLimit¶
-
CylindricalJointBuilder.
EnableLinearLowerLimit
¶ Returns or sets the linear lower limit option.
If the enable is true, then this joint will be applied the lower limit in linear direction.
-------------------------------------
Getter Method
Signature
EnableLinearLowerLimit()
Returns: Return type: bool New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
EnableLinearLowerLimit(enable)
Parameters: enable (bool) – New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
EnableLinearUpperLimit¶
-
CylindricalJointBuilder.
EnableLinearUpperLimit
¶ Returns or sets the linear upper limit option.
If the enable is true, then this joint will be applied the upper limit in linear direction.
-------------------------------------
Getter Method
Signature
EnableLinearUpperLimit()
Returns: Return type: bool New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
EnableLinearUpperLimit(enable)
Parameters: enable (bool) – New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
LinearLowerLimit¶
-
CylindricalJointBuilder.
LinearLowerLimit
¶ Returns the linear lower limit.
The lower limit setup for joint linear movement.
-------------------------------------
Getter Method
Signature
LinearLowerLimit()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
LinearUpperLimit¶
-
CylindricalJointBuilder.
LinearUpperLimit
¶ Returns the linear upper limit.
The upper limit setup for joint linear movement.
-------------------------------------
Getter Method
Signature
LinearUpperLimit()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Offset¶
-
CylindricalJointBuilder.
Offset
¶ Returns the offset value.
-------------------------------------
Getter Method
Signature
Offset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
StartAngle¶
-
CylindricalJointBuilder.
StartAngle
¶ Returns the start angle.
-------------------------------------
Getter Method
Signature
StartAngle()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Validate¶
-
CylindricalJointBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.