ComparisonResultElectricalPart Class¶
-
class
NXOpen.Mechatronics.
ComparisonResultElectricalPart
¶ Bases:
NXOpen.Mechatronics.ComparisonResultBase
Represents electrical part of comparison result
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ComparisonStatus | Returns the status from the electrical part |
Ignored | Returns or sets the flag marked if the object will be ingored when applying it to logical model |
PartNumber | Returns the part number from the electrical part |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetAttributes | Gets a list of attributes from the electrical part |
Enumerations¶
ComparisonResultElectricalPartStatus Enumeration | Defines statuses of electrical parts |
Property Detail¶
ComparisonStatus¶
-
ComparisonResultElectricalPart.
ComparisonStatus
¶ Returns the status from the electrical part
-------------------------------------
Getter Method
Signature
ComparisonStatus()
Returns: Status of electrical part Return type: NXOpen.Mechatronics.ComparisonResultElectricalPartStatus
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Dispose¶
-
ComparisonResultElectricalPart.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX9.0.0.
License requirements: None.
GetAttributes¶
-
ComparisonResultElectricalPart.
GetAttributes
¶ Gets a list of attributes from the electrical part
Signature
GetAttributes()
Returns: a tuple Return type: A tuple consisting of (attributeNames, attributeValues). attributeNames is a list of str. Array of attribute names attributeValues is a list of str. Array of attribute values New in version NX9.0.0.
License requirements: None.