ComparisonResultElectricalPartStatus Enumeration

NXOpen.Mechatronics.ComparisonResultElectricalPart.Status is an alias for NXOpen.Mechatronics.ComparisonResultElectricalPartStatus

class NXOpen.Mechatronics.ComparisonResultElectricalPartStatus

Bases: object

Defines statuses of electrical parts

Enum Members

Enum Member Enum Member Description
Added
Added status
Removed
Removed status
Updated
Updated status
Identical
Identical status
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.