CollisionShapeBuilder Class¶
-
class
NXOpen.Mechatronics.
CollisionShapeBuilder
¶ Bases:
NXOpen.Builder
This is an abstract class, and cannot be created.
This is an abstract class, and cannot be created.
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
CenterPoint | Returns or sets the center point. |
Height | Returns the height. |
Length | Returns the length. |
Orientation | Returns or sets the orientation. |
Radius | Returns the radius. |
Tag | Returns the Tag for this object. |
Width | Returns the width. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CenterPoint¶
-
CollisionShapeBuilder.
CenterPoint
¶ Returns or sets the center point.
Valid to all collsion shape types except
NXOpen.Mechatronics.CollisionBodyBuilder.CollisionShape()
is set toNXOpen.Mechatronics.CollisionBodyBuilderCollisionShapeTypes.Convex
.-------------------------------------
Getter Method
Signature
CenterPoint()
Returns: Return type: NXOpen.Point
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
CenterPoint(centerPoint)
Parameters: centerPoint ( NXOpen.Point
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Height¶
-
CollisionShapeBuilder.
Height
¶ Returns the height.
Valid if
NXOpen.Mechatronics.CollisionBodyBuilder.CollisionShape()
is set toNXOpen.Mechatronics.CollisionBodyBuilderCollisionShapeTypes.Box
orNXOpen.Mechatronics.CollisionSensorBuilder.CollisionShape()
is set toNXOpen.Mechatronics.CollisionSensorBuilderCollisionShapeTypes.Box
.-------------------------------------
Getter Method
Signature
Height()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Length¶
-
CollisionShapeBuilder.
Length
¶ Returns the length.
Valid if
NXOpen.Mechatronics.CollisionBodyBuilder.CollisionShape()
is set toNXOpen.Mechatronics.CollisionBodyBuilderCollisionShapeTypes.Box
orNXOpen.Mechatronics.CollisionBodyBuilderCollisionShapeTypes.Capsule
orNXOpen.Mechatronics.CollisionSensorBuilder.CollisionShape()
is set toNXOpen.Mechatronics.CollisionSensorBuilderCollisionShapeTypes.Box
orNXOpen.Mechatronics.CollisionSensorBuilderCollisionShapeTypes.Line
.-------------------------------------
Getter Method
Signature
Length()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Orientation¶
-
CollisionShapeBuilder.
Orientation
¶ Returns or sets the orientation.
Valid if
NXOpen.Mechatronics.CollisionBodyBuilder.CollisionShape()
is set toNXOpen.Mechatronics.CollisionBodyBuilderCollisionShapeTypes.Box
orNXOpen.Mechatronics.CollisionBodyBuilderCollisionShapeTypes.Capsule
orNXOpen.Mechatronics.CollisionSensorBuilder.CollisionShape()
is set toNXOpen.Mechatronics.CollisionSensorBuilderCollisionShapeTypes.Box
orNXOpen.Mechatronics.CollisionSensorBuilderCollisionShapeTypes.Line
.-------------------------------------
Getter Method
Signature
Orientation()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Orientation(orientation)
Parameters: orientation ( NXOpen.CoordinateSystem
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Radius¶
-
CollisionShapeBuilder.
Radius
¶ Returns the radius.
Valid if
NXOpen.Mechatronics.CollisionBodyBuilder.CollisionShape()
is set toNXOpen.Mechatronics.CollisionBodyBuilderCollisionShapeTypes.Sphere
orNXOpen.Mechatronics.CollisionSensorBuilder.CollisionShape()
is set toNXOpen.Mechatronics.CollisionSensorBuilderCollisionShapeTypes.Sphere
.-------------------------------------
Getter Method
Signature
Radius()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Width¶
-
CollisionShapeBuilder.
Width
¶ Returns the width.
Valid if
NXOpen.Mechatronics.CollisionBodyBuilder.CollisionShape()
is set toNXOpen.Mechatronics.CollisionBodyBuilderCollisionShapeTypes.Box
orNXOpen.Mechatronics.CollisionSensorBuilder.CollisionShape()
is set toNXOpen.Mechatronics.CollisionSensorBuilderCollisionShapeTypes.Box
.-------------------------------------
Getter Method
Signature
Width()
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Validate¶
-
CollisionShapeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.