CollisionSensorBuilderCollisionShapeTypes Enumeration

NXOpen.Mechatronics.CollisionSensorBuilder.CollisionShapeTypes is an alias for NXOpen.Mechatronics.CollisionSensorBuilderCollisionShapeTypes

class NXOpen.Mechatronics.CollisionSensorBuilderCollisionShapeTypes

Bases: object

the Trigger Shape Types.

Enum Members

Enum Member Enum Member Description
Box
Box
Sphere
Sphere
Line
Line
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.