IssueAttachment Class |
Represents the Issue Attachment object. |
IssueBriefcase Class |
Represents the Issue Briefcase object. |
IssueBriefcaseSynchronizeBuilder Class |
Represents a NXOpen.Issue.IssueBriefcase synchronize builder |
IssueContent Class |
Represents the Issue Issue object. |
IssueContentBuilder Class |
Represents a NXOpen.Issue.IssueContent builder |
IssueFolder Class |
Represents the Issue Folder object. |
IssueList Class |
Represents the Issue List object. |
IssueListCollection Class |
Represents a NXOpen.Issue.IssueListCollection |
IssueManager Class |
Contains the collection objects for creating and iterating over issue objects. |
IssueProperty Class |
Represents the Issue Property object. |
IssueSite Class |
Represents the Issue Site object. |
SnapshotSubsetBuilder Class |
Used to create or edit issue snapshot subset. |
SnapshotWorksetBuilder Class |
Used to create or edit issue snapshot workset which is a container to hold all the corresponding parts to represent an issue. |