IssueAttachmentType Enumeration¶
NXOpen.Issue.IssueAttachment.Type is an alias for NXOpen.Issue.IssueAttachmentType
-
class
NXOpen.Issue.
IssueAttachmentType
¶ Bases:
object
Represents the possible attachment types for a
NXOpen.Issue.IssueAttachment
.Enum Members
Enum Member Enum Member Description Generic Generic typeText Text typePart Part typeXml XML typeImage Image typeValidationLog Validation log fileBookmark Bookmark typeSnapshot Snapshot typeValidationResult ValidationResult object typeWorkset Workset typeShapeDesignElement Shape Design Element typeReuseDesignElement Reuse Design Element typeSubordinateDesignElement Subordinate Design Element typePromissoryDesignElement Promissory Design Element typeDesignControlElement Design Control Element typeSubset Subset typeMSWord Microsoft Word typeMSExcel Microsoft Excel typeMSPowerPoint Microsoft Power Point type-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-