IGenericFileNewApplicationBuilder Class¶
-
class
NXOpen.Gateway.
IGenericFileNewApplicationBuilder
¶ Bases:
NXOpen.Builder
,NXOpen.IAttributeSourceObjectBuilder
Represents the class Application Builder.
Instances of this class can be accessed through various application specific builders
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
AutoAssignAttributes | Auto assigns the attributes for a given array of objects and returns an array of objects that failed to auto assign. |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
AutoAssignAttributes¶
-
IGenericFileNewApplicationBuilder.
AutoAssignAttributes
¶ Auto assigns the attributes for a given array of objects and returns an array of objects that failed to auto assign.
Signature
AutoAssignAttributes(objects)
Parameters: objects (list of NXOpen.NXObject
) –Returns: Return type: NXOpen.ErrorList
New in version NX8.5.0.
License requirements: None.
Validate¶
-
IGenericFileNewApplicationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.